<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Memory Configuration Editor not working</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568152#M19198</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by whitecoe on Fri Apr 26 07:26:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Why not try importing one of the supplied memconfig xml files?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.support.code-red-tech.com/CodeRedWiki/MemoryConfigEditing&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;HTH!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:02:56 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:02:56Z</dc:date>
    <item>
      <title>Memory Configuration Editor not working</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568151#M19197</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jcottier on Fri Apr 26 06:22:20 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, I am using LPCXpresso v5.2.2 [Build 2108] [2013-04-17] on Ubuntu 12.04 (32 bit) for an LPC4357 based project (element14 evaluation board).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the Memory Configuration Editor to "Add flash" so I can&amp;nbsp; add an SPIFlash memory section, but when I enter the "Location" value (0x14000000), then I get an error "Invalid memory configuration, flash overlaps with RamLoc32" message box. RamLoc32 location = 0x10000000 and size = 0x8000, so they do not appear to overlap. However the "Location" value I entered now appears in the size field instead, with the location value now showing as 0x0. Is this a bug? or am I doing something wrong?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568151#M19197</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:02:55Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Configuration Editor not working</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568152#M19198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by whitecoe on Fri Apr 26 07:26:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Why not try importing one of the supplied memconfig xml files?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.support.code-red-tech.com/CodeRedWiki/MemoryConfigEditing&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;HTH!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568152#M19198</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Configuration Editor not working</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568153#M19199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jcottier on Tue Apr 30 02:44:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi whitcoe, that seems to works ok. I was just following turorial for SPIFI operation. I have tried the editor in Lpcxpresso v4 and it works fine so it seems there is a bug in the latest Eclipse used on v5. However I cannot get the program to run from SPIFI, one of the consoles messages showed a problem with licensing but I cannot back to that console at the end of the compile/link process. Can you tell me if there is a log or a way to re-open a closed console?.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:02:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568153#M19199</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:02:57Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Configuration Editor not working</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568154#M19200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Wed May 01 02:07:53 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The issue with the memory configuration editor should be fixed in LPCXpresso 5.2.4, which has just been released. More information in:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?t=4474&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:02:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Memory-Configuration-Editor-not-working/m-p/568154#M19200</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:02:57Z</dc:date>
    </item>
  </channel>
</rss>