<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LCP11u14 ADC in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567493#M18907</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by madid87 on Wed Feb 13 02:22:08 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can put an input amplifier which would translate your signal to the desired range.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:45:17 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:45:17Z</dc:date>
    <item>
      <title>LCP11u14 ADC</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567492#M18906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Frankb on Wed Feb 13 02:09:27 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use the ADC on a LPC11u14 microprocessor. Now I found that it has a 10 bit resolution and has an input voltage of 0.0 - 3.6V. Now I have an analog sensor that outputs 0.3 - 3.0V, which means that I would loose around a third of my resolution. Is it possible to change the range of the ADC from 0.0 - 3.6V to 0.3 - 3.0V so that I make full use of the 10 bits resolution?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567492#M18906</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: LCP11u14 ADC</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567493#M18907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by madid87 on Wed Feb 13 02:22:08 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can put an input amplifier which would translate your signal to the desired range.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567493#M18907</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:45:17Z</dc:date>
    </item>
    <item>
      <title>Re: LCP11u14 ADC</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567494#M18908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ex-kayoda on Wed Feb 13 03:18:22 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Frankb&lt;/STRONG&gt;&lt;BR /&gt;... input voltage of 0.0 - 3.6V...&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Isn't VREF = VDD :confused:&amp;nbsp; So your resolution depends on your VDD. If you choose 3.0V you lose only 10% ;)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LCP11u14-ADC/m-p/567494#M18908</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:45:18Z</dc:date>
    </item>
  </channel>
</rss>