<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: USB_FTOGGLE usage</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567482#M18903</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Jun 07 22:31:39 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Usually this pin is used (as input) to use MSC (USB Bootloader).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's not needed (as output) for general USB function :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;8.4.1 LQFP48 packages&lt;BR /&gt;Table 144. LPC1313/42/43 LQFP48 pin description table&lt;BR /&gt;&lt;BR /&gt;PIO0_1/CLKOUT/CT32B0_MAT2/USB_FTOGGLE&lt;BR /&gt;4[3] yes I/O I; PU PIO0_1 — General purpose digital input/output pin. A LOW level on this pin during reset starts the ISP command handler or the USB device enumeration (USB on LPC1343 only, see description of PIO0_3).&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:20:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:20:30Z</dc:date>
    <item>
      <title>USB_FTOGGLE usage</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567481#M18902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mtburt on Thu Jun 07 22:04:49 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm starting a new design with the LPC1343 and using the USB device peripheral.&amp;nbsp; I'm trying to finish up the schematic and can't seem to find how the USB_FTOGGLE pin is intended to be used.&amp;nbsp; From the user manual it looks like it's an output that toggles on the USB 1ms start-of-frame signal.&amp;nbsp; But I don't understand if there is some external trigger on that event or some other action that should be performed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I just want to verify that I'm safe ignoring this output in my design.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-Matt&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567481#M18902</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: USB_FTOGGLE usage</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567482#M18903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Jun 07 22:31:39 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Usually this pin is used (as input) to use MSC (USB Bootloader).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It's not needed (as output) for general USB function :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;8.4.1 LQFP48 packages&lt;BR /&gt;Table 144. LPC1313/42/43 LQFP48 pin description table&lt;BR /&gt;&lt;BR /&gt;PIO0_1/CLKOUT/CT32B0_MAT2/USB_FTOGGLE&lt;BR /&gt;4[3] yes I/O I; PU PIO0_1 — General purpose digital input/output pin. A LOW level on this pin during reset starts the ISP command handler or the USB device enumeration (USB on LPC1343 only, see description of PIO0_3).&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567482#M18903</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: USB_FTOGGLE usage</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567483#M18904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Tsuneo on Fri Jun 08 18:01:38 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;USB_FTOGGLE pin of LPC13xx is an output-only pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This pin is supposed for USB Audio application, to synchronize external components (S/PDIF transceiver, MP3 codec, etc.) to the bus timing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tsuneo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/USB-FTOGGLE-usage/m-p/567483#M18904</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:20:31Z</dc:date>
    </item>
  </channel>
</rss>