<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックProblems when flashing NGX LPC4330-Xplorer</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problems-when-flashing-NGX-LPC4330-Xplorer/m-p/567464#M18897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Reinhard Huck on Thu Feb 04 08:43:33 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to flash an application to the NGX LPC4330-Xplorer board using LPCXpresso v8.0.0 [Build 526] [2015-11-23] on Windows 10 64 Bit. During the flash process I get the following error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Error in final launch sequence&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Failed to execute MI command:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-target-download&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Error message from debugger back end:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Could not write registers; remote failure reply 'E22'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Could not write registers; remote failure reply 'E22'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my question is: How to flash the NGX LPC4330-Xplorer board using LPCXpresso v8.0.0 (is there something to be considered)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Reinhard&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:24:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:24:50Z</dc:date>
    <item>
      <title>Problems when flashing NGX LPC4330-Xplorer</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problems-when-flashing-NGX-LPC4330-Xplorer/m-p/567464#M18897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Reinhard Huck on Thu Feb 04 08:43:33 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to flash an application to the NGX LPC4330-Xplorer board using LPCXpresso v8.0.0 [Build 526] [2015-11-23] on Windows 10 64 Bit. During the flash process I get the following error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Error in final launch sequence&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Failed to execute MI command:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-target-download&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Error message from debugger back end:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Could not write registers; remote failure reply 'E22'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Could not write registers; remote failure reply 'E22'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my question is: How to flash the NGX LPC4330-Xplorer board using LPCXpresso v8.0.0 (is there something to be considered)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Reinhard&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problems-when-flashing-NGX-LPC4330-Xplorer/m-p/567464#M18897</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:24:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problems when flashing NGX LPC4330-Xplorer</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problems-when-flashing-NGX-LPC4330-Xplorer/m-p/567465#M18898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 04 10:30:39 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I presume you've connected an external debug probe? You didn't mention any details about the LPC-Link2 (or other) probe connection. Can you post the project debug log in your reply?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problems-when-flashing-NGX-LPC4330-Xplorer/m-p/567465#M18898</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:24:51Z</dc:date>
    </item>
  </channel>
</rss>