<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Vector Table Offset in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Vector-Table-Offset/m-p/566297#M18381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by igorsk on Fri May 13 05:53:11 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It allows you to change/set up the vectors dynamically (can be useful in some cases). It's also the only way to go if you have a custom bootloader which runs an application flashed at another address - the vectors need to be changed to the application's but the 0-base vectors are taken by the bootloader.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:44:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:44:50Z</dc:date>
    <item>
      <title>Vector Table Offset</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Vector-Table-Offset/m-p/566296#M18380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by affonpign on Fri May 13 05:02:05 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What advantage do I have to remap the interrupt vector table to the SRAM. I understands how it works but I do not see the use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;affonpign&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Vector-Table-Offset/m-p/566296#M18380</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: Vector Table Offset</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Vector-Table-Offset/m-p/566297#M18381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by igorsk on Fri May 13 05:53:11 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It allows you to change/set up the vectors dynamically (can be useful in some cases). It's also the only way to go if you have a custom bootloader which runs an application flashed at another address - the vectors need to be changed to the application's but the 0-base vectors are taken by the bootloader.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Vector-Table-Offset/m-p/566297#M18381</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:44:50Z</dc:date>
    </item>
  </channel>
</rss>