<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SWD connections? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566122#M18304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Thu Apr 22 19:42:54 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The latest LPC111x user manual, rev 00.12, says that only two connections are necessary for the SWD interface. They are SWCLK and SWDIO and ground, of course.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However the shematic for the LPCXpresso board show those connections and two more. RESET with a 12K resistor pull-up is connected and SWO is connected to pin 29. There is a note that says "SWO does not exist on LPC1114", but is is connected never the less.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Do those additional lines serve some function? Is there a reason to connect them if the pins are not otherwise needed?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:18:14 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:18:14Z</dc:date>
    <item>
      <title>SWD connections?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566122#M18304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Thu Apr 22 19:42:54 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The latest LPC111x user manual, rev 00.12, says that only two connections are necessary for the SWD interface. They are SWCLK and SWDIO and ground, of course.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;However the shematic for the LPCXpresso board show those connections and two more. RESET with a 12K resistor pull-up is connected and SWO is connected to pin 29. There is a note that says "SWO does not exist on LPC1114", but is is connected never the less.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Do those additional lines serve some function? Is there a reason to connect them if the pins are not otherwise needed?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566122#M18304</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:18:14Z</dc:date>
    </item>
    <item>
      <title>Re: SWD connections?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566123#M18305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by igorsk on Fri Apr 23 05:15:47 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;SWO is used on LPC13xx, and the same board layout is used for both chips.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566123#M18305</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:18:15Z</dc:date>
    </item>
    <item>
      <title>Re: SWD connections?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566124#M18306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Fri Apr 23 07:59:28 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The question that I have; is there any value in connecting the RESET line on a LPC111x series chip?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566124#M18306</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: SWD connections?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566125#M18307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Apr 23 10:57:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: micrio&lt;/STRONG&gt;&lt;BR /&gt;The question that I have; is there any value in connecting the RESET line on a LPC111x series chip?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPCXpresso IDE has reason to pull RESET under certain circumstances. Please connect it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SWD-connections/m-p/566125#M18307</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:18:16Z</dc:date>
    </item>
  </channel>
</rss>