<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: LPC1769 blinky error.</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565631#M18091</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by behzat_c on Tue May 17 14:24:58 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I used the example coming from the Eclipse project which is under the name of GPIO.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the other hand,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I managed to find the real CMSIS from &lt;/SPAN&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/zip/lpc17xx.cmsis.driver.library.zip&lt;/A&gt;&lt;SPAN&gt; . I say real because the one comes with the Ecplise doesn't include peripheral support but this one have.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But, in this case i couldn't find a way to use this library with Eclipse LPCXpresso environment.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:41:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:41:52Z</dc:date>
    <item>
      <title>LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565626#M18086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by behzat_c on Tue May 17 10:54:32 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCXpresso LPC1769 board with LPCXpresso Code RED Eclipse IDE.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm a newbie for this platform and couldn't make the onboard led blink. I uploaded the GPIO example into board with changing the port but nothing happened.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also found the example is quite complex. Is there any ready made easy to use libraries out there?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, what is interesting is that, onboard LED is constantly on even i upload an empty program into the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Problem solved. I was dealing with the wrong pin number from the start. I changed it and worked.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;By the way, i'm still searching for a good library/functions to use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565626#M18086</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565627#M18087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larryvc on Tue May 17 11:25:58 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: behzat_c&lt;/STRONG&gt;&lt;BR /&gt; &lt;BR /&gt;By the way, i'm still searching for a good library/functions to use.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The rest of us are too.:rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What specifically are you looking to find in the way of libraries and functions?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565627#M18087</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565628#M18088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by behzat_c on Tue May 17 12:55:11 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Especcially for peripheral settings. For example setting a pin's function, input/output charachteristic, initializing UART or reading an ADC value shouldn't be so hard.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;All examples include evil bit level hackings, pointer conversions and etc. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There should be easy way. 8 bit micros. can be shown as example for library simplicity.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565628#M18088</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565629#M18089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larryvc on Tue May 17 13:49:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: behzat_c&lt;/STRONG&gt;&lt;BR /&gt;Especcially for peripheral settings. For example setting a pin's function, input/output charachteristic, initializing UART or reading an ADC value shouldn't be so hard.&lt;BR /&gt; &lt;BR /&gt;All examples include evil bit level hackings, pointer conversions and etc. &lt;BR /&gt; &lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I said, I haven't seen any specific libraries to use either.&amp;nbsp; You have to remember that this is a free development environment that CodeRed has provided us.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The CMSIS library does contain definitions for the device and peripherals but in itself it is not a library of functions as you are referring to.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Almost everybody here has had to learn about the peripheral and device settings by using the examples provided within LPCXpresso.&amp;nbsp; The best advice I can offer you is to study and use the examples and CMSIS and read the UM10360 user manual.&amp;nbsp; Trust me, you will have to read it many times.:)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The user manual can be found here:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/pdf/user.manual.lpc17xx.pdf&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps someone else has more information to provide you.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565629#M18089</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565630#M18090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larryvc on Tue May 17 14:05:34 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: behzat_c&lt;/STRONG&gt;&lt;BR /&gt; &lt;BR /&gt;I also found the example is quite complex. &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I forgot to ask.&amp;nbsp; Which GPIO example are you referring to?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565630#M18090</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565631#M18091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by behzat_c on Tue May 17 14:24:58 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I used the example coming from the Eclipse project which is under the name of GPIO.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;On the other hand,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I managed to find the real CMSIS from &lt;/SPAN&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/zip/lpc17xx.cmsis.driver.library.zip&lt;/A&gt;&lt;SPAN&gt; . I say real because the one comes with the Ecplise doesn't include peripheral support but this one have.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But, in this case i couldn't find a way to use this library with Eclipse LPCXpresso environment.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565631#M18091</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 blinky error.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565632#M18092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by larryvc on Tue May 17 14:42:08 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I think CodeRedSupport may have to provide you with guidance on how to start off using LPCXpresso and CMSIS.&amp;nbsp; There are differences between the examples that NXP and CodeRed provide.&amp;nbsp; These can lead to confusion.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You should start off by only using the simple examples within LPCXPresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Under Quickstart find Import example project(s) and browse to the LPC17xx folder and import all the files in LPCXpresso1768.zip.&amp;nbsp; Then look at the LPCXpresso1768_systick example.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-blinky-error/m-p/565632#M18092</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:41:53Z</dc:date>
    </item>
  </channel>
</rss>