<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: LPC1317 external memory interface</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1317-external-memory-interface/m-p/565400#M17977</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by frame on Tue Apr 30 05:08:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Any pin to pin compatible NXP series MCU&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;IMHO, this is the only viable hardware option.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I don't know the other requirements of your project, it is up to you to check for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;such an MCU with increased Flash size.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Trying to implement some code swap solution via SD card or other IO channel is a bad idea.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Not only will it consume even more space in Flash for the swap management, but also bust&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;your project budget in development costs, because of exponentially increased complexity.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And if you need to swap code under any kind of real-time requirements, it gets even worse.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Some other thing you can try - another toolchain.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not really a big fan of Keil uVision, but I have experienced a reduction in code size&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;down to 50...60% for identical settings, when compared with GCC based toolchains.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ant I'm having a paid licence for one of the latter.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:57:20 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:57:20Z</dc:date>
    <item>
      <title>LPC1317 external memory interface</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1317-external-memory-interface/m-p/565399#M17976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aamir ali on Tue Apr 30 04:01:04 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC1317 for one of my project &amp;amp; I am falling short of flash as project is bigger. Now changing controller is difficult.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can I store code in some external memory &amp;amp; then call it. I have still 5K of Ram left-&amp;gt; 3K in SRAM0 &amp;amp; 2K in SRAM1 &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have external SDHC card interface with SPI interface with 18Mhz. Can it help in any way, or any other memory interface to solve the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;OR&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any pin to pin compatible NXP series MCU&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am running my system at 72Mhz/3.3V.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;CRITICAL FOR MY APP:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1317-external-memory-interface/m-p/565399#M17976</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1317 external memory interface</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1317-external-memory-interface/m-p/565400#M17977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by frame on Tue Apr 30 05:08:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Any pin to pin compatible NXP series MCU&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;IMHO, this is the only viable hardware option.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I don't know the other requirements of your project, it is up to you to check for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;such an MCU with increased Flash size.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Trying to implement some code swap solution via SD card or other IO channel is a bad idea.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Not only will it consume even more space in Flash for the swap management, but also bust&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;your project budget in development costs, because of exponentially increased complexity.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And if you need to swap code under any kind of real-time requirements, it gets even worse.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Some other thing you can try - another toolchain.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not really a big fan of Keil uVision, but I have experienced a reduction in code size&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;down to 50...60% for identical settings, when compared with GCC based toolchains.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ant I'm having a paid licence for one of the latter.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1317-external-memory-interface/m-p/565400#M17977</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:57:20Z</dc:date>
    </item>
  </channel>
</rss>