<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Using On-Chip USB Driver for Communications via virtual COM Port</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565301#M17933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Sakphul on Sat May 14 09:01:50 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;is it possible to use the On Chip USB Driver within the ROM for Communication via a Virtual COM Port?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen the usbcdc example using a self written usb Driver which consumes about 6kB of Flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to use the on-Chip USB Driver instead of this self written one. But within the Users manual of the LPC1343 it says that the On-Chip Driver only supports HID and MSC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So is it possible to run a communications connection with the On-Chip Driver just by changing the USB Device Descriptor?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:44:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:44:39Z</dc:date>
    <item>
      <title>Using On-Chip USB Driver for Communications via virtual COM Port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565301#M17933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Sakphul on Sat May 14 09:01:50 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;is it possible to use the On Chip USB Driver within the ROM for Communication via a Virtual COM Port?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have seen the usbcdc example using a self written usb Driver which consumes about 6kB of Flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to use the on-Chip USB Driver instead of this self written one. But within the Users manual of the LPC1343 it says that the On-Chip Driver only supports HID and MSC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So is it possible to run a communications connection with the On-Chip Driver just by changing the USB Device Descriptor?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565301#M17933</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Using On-Chip USB Driver for Communications via virtual COM Port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565302#M17934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ktownsend on Sat May 14 09:42:32 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Sakphul&lt;/STRONG&gt;&lt;BR /&gt;Hello&lt;BR /&gt;is it possible to use the On Chip USB Driver within the ROM for Communication via a Virtual COM Port?&lt;BR /&gt;I have seen the usbcdc example using a self written usb Driver which consumes about 6kB of Flash.&lt;BR /&gt;I would like to use the on-Chip USB Driver instead of this self written one. But within the Users manual of the LPC1343 it says that the On-Chip Driver only supports HID and MSC.&lt;BR /&gt; &lt;BR /&gt;So is it possible to run a communications connection with the On-Chip Driver just by changing the USB Device Descriptor?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Generally, the UM doesn't (intentionally) lie. :)&amp;nbsp; You can only use the on-chip drivers for HID and MSC.&amp;nbsp; If you want CDC, etc., you'll have to roll your own.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565302#M17934</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:44:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using On-Chip USB Driver for Communications via virtual COM Port</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565303#M17935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Sakphul on Sat May 14 09:46:14 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ok, then another Question:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For Debugging Purposes i would like print some Test strings via USB. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there any tool out there where i can log/see the data transmitted by a HID Device? Like a terminal programm for RS232? Or do i have to write my own Programm for that?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Using-On-Chip-USB-Driver-for-Communications-via-virtual-COM-Port/m-p/565303#M17935</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:44:41Z</dc:date>
    </item>
  </channel>
</rss>