<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Deep sleep on LPC11U14</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Deep-sleep-on-LPC11U14/m-p/565226#M17893</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Muis on Thu Jan 03 08:52:30 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I developed a simple datalogger using the LPC11U24. It records 256 samples per second, and goes to sleep using __WFI(); in between samples. It currently consumes about 2 mA (at 12 Mhz), which seems to match the datasheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To further reduce power consumption I'd like to use deep-sleep, and for the LPC1114 there is a &lt;/SPAN&gt;&lt;A href="http://http://ics.nxp.com/support/lpcxpresso/zip/examples.lpc1114.timed.wakeup.zip"&gt;perfect example&lt;/A&gt;&lt;SPAN&gt;, but for the LPC11U14 there is no 'timed wakeup' example, and since it features a different watchdog (WDT vs WWDT) i cannot port the code easily.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does someone have a timed wakeup example for the LPC11U14?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:24:41 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:24:41Z</dc:date>
    <item>
      <title>Deep sleep on LPC11U14</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Deep-sleep-on-LPC11U14/m-p/565226#M17893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Muis on Thu Jan 03 08:52:30 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I developed a simple datalogger using the LPC11U24. It records 256 samples per second, and goes to sleep using __WFI(); in between samples. It currently consumes about 2 mA (at 12 Mhz), which seems to match the datasheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To further reduce power consumption I'd like to use deep-sleep, and for the LPC1114 there is a &lt;/SPAN&gt;&lt;A href="http://http://ics.nxp.com/support/lpcxpresso/zip/examples.lpc1114.timed.wakeup.zip"&gt;perfect example&lt;/A&gt;&lt;SPAN&gt;, but for the LPC11U14 there is no 'timed wakeup' example, and since it features a different watchdog (WDT vs WWDT) i cannot port the code easily.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does someone have a timed wakeup example for the LPC11U14?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Deep-sleep-on-LPC11U14/m-p/565226#M17893</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:24:41Z</dc:date>
    </item>
  </channel>
</rss>