<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Schema for USB host port configuration in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565164#M17867</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DavidLola on Mon Apr 28 02:02:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;And at the same time, if i don't have the LM3526-L, is the schema still running or not?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:43:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:43:43Z</dc:date>
    <item>
      <title>Schema for USB host port configuration</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565163#M17866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DavidLola on Mon Apr 28 02:00:14 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the datasheet of NXP1769, there is a schema for USB host port configuration, but i don't understand is why there is no 5 V for the USB-A connector. The USB_PWRD which is connected with Vbus is not 5V. So what is the real schema for USB host port configuration?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565163#M17866</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:43:42Z</dc:date>
    </item>
    <item>
      <title>Re: Schema for USB host port configuration</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565164#M17867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DavidLola on Mon Apr 28 02:02:36 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;And at the same time, if i don't have the LM3526-L, is the schema still running or not?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565164#M17867</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:43:43Z</dc:date>
    </item>
    <item>
      <title>Re: Schema for USB host port configuration</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565165#M17868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Mon Apr 28 08:09:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Assuming you're referring to Figure 31, "USB host port configuration".&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As I understand the schematics, is that VBUS is connected to LM3526's OUTA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The LM3526 would be connected to +5V and the microcontroller's USB_PPWR and USB_OVRCR.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;USB_PPWR is "port power enable", USB_OVRCR is "over-current status". USB_PWRD is "port power status".&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps you didn't notice the difference between PPWR and PWRD ? :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, I believe it would probably work (temporarily) if you connect it to +5V via a 500mA fuse, until you get your USB-power-switch, which is what LM3526-L is.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There are many alternatives to LM3526-L; I'm personally considering Micrel's MIC2005A-2YM6.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have not verified if it will work, though, but the price isn't too high.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565165#M17868</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: Schema for USB host port configuration</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565166#M17869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by DavidLola on Mon Apr 28 08:26:28 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you first for your answer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Normally, the Vbus of the USB-A connector should be connected to a 5V tension(in a host mode), is that right?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So i didn't connect the Vbus to the LM3526's OUTA and USB_PWRD, but to a 5V tension.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And i use the example of LPCopen mass storage host, the board is LPC1769 REV B.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But it doesn't work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you tell me what's the problem?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565166#M17869</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: Schema for USB host port configuration</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565167#M17870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Mon Apr 28 10:10:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hmm, I don't want you to fry your LPC, so I'll ask if you could post a schematic of your current USB-connection to the LPC ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Schema-for-USB-host-port-configuration/m-p/565167#M17870</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:43:45Z</dc:date>
    </item>
  </channel>
</rss>