<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックdetecting usb attachment</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564984#M17822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jjsd on Tue Aug 16 10:22:04 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCXpresso v3.6.3_317 with a LPC1754 micro in a CDC virtual comm port application using the LPC1700_usbstack example code for the CDC support. The micro board is self-powered.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a way to detect on the micro side when the host computer has attached and enumerated the usb? Looking basically to generate a flag that indicates the port is open and ready or not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:21:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:21:43Z</dc:date>
    <item>
      <title>detecting usb attachment</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564984#M17822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jjsd on Tue Aug 16 10:22:04 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using LPCXpresso v3.6.3_317 with a LPC1754 micro in a CDC virtual comm port application using the LPC1700_usbstack example code for the CDC support. The micro board is self-powered.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a way to detect on the micro side when the host computer has attached and enumerated the usb? Looking basically to generate a flag that indicates the port is open and ready or not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564984#M17822</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:21:43Z</dc:date>
    </item>
    <item>
      <title>Re: detecting usb attachment</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564985#M17823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Tue Aug 16 23:13:29 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;J.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;this all depends on the USB stack you are using (or actually not ...)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The Keil example (the one named usbcdc) shows the use of the global USB_Configuration variable (or should I say misused) to detect if the device is connected. USB_Configurations is given a value somewhere during the initialization process but I have no idea when...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I use the USB stack from Bertrik Sikken which can be found in the RDB1768cmsis examples. This stack has a number of advantages over the Keil stack. For one it has no limitations on distribution as either binary or source code (you are not allowed to distribute source code of the Keil stack) but it is also much nicer to configure.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you look at the usb_serial example in the mentioned example set, you'll see that almost everything is placed in main_serial.c.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the main() function USB is initialized and the interrupt handlers for the endpoints are registered.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am not sure how familiar you are with USB, I will try (if not for you then maybe for others who read this :rolleyes:) to explain very shortly how USB is used.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;During initialization the host reads the device descriptors of the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;These descriptors contain the information about the device (ID, serial no., name, device type, ...) including information on the end points.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;End points are the main interface between the USB host and your application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For the CDC There are two end points: BULK_IN_EP and BULK_OUT_EP. The host (PC) reads the BULK_IN and writes to BULK_OUT in certain intervals (as configured in the device descriptors).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This bulk end points contain 0 or more bytes of data, any characters send towards the PC are to be placed in the IN end point (IN for the PC), any characters send from the PC are received in the OUT end point.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you look at the source you will see that there are two functions BulkIn() and BulkOut(), these are being called by the USB stack to tell the program USB want to read or write data.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A third function that might be of interest is HandleClassRequest(). This function is called when the PC wants to configure the (virtual) serial port (e.g. set the baud rate).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is (almost) all you need to know about USB, most USB devices work in a similar way. End points may vary in type and number and the HandleClassRequest of course contains different requests depending of the device but as you look at the different USB examples (in the RDB1768cmsis examples) you will see how this is done.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Knowing this, it is a simple task to include your own 'Yes, we are alive!" checks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You can set a flag as soon as you the BulkIn() function is called. This then signals that the PC is now polling your device for data.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You can also set a flag when HandleClassRequest() is called, but you have to try a bit to see if, and when, this function is called. I am not sure if this function is always called or at what time it is called.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I do not know is if there are ways to tell if an application has the device open or not. I.e: I have my device attached to the PC, open a (terminal) program that uses the device, close the program, open it again, etc...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have not checked if this open/close sequence is visible on the lpc1754 side of the USB stack.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This should also be possible with the Keil stack but I have no idea where this is placed inside the code of that stack.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope this helps.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,[INDENT]Rob&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/INDENT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564985#M17823</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: detecting usb attachment</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564986#M17824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jjsd on Mon Aug 22 11:47:48 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have something working now. Not perfect, but works. I'm using the USB stack from Bertrik Sikke.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I&amp;nbsp; added a variable, uint8_t vcom_portOpen, to act as a flag, initialized&amp;nbsp; to FALSE. I modified the HandleClassRequest and USBHwISR functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There&amp;nbsp; is a sequence of usb activity that occurs when a port is opened. On&amp;nbsp; Windows XP and 7 it looks like the sequence of activity appears to be&amp;nbsp; the same, but I'm apprehensive to count on it. The amount of time the&amp;nbsp; sequence takes before the port is actually open varies with the host&amp;nbsp; computer speed. Among other things several HandleClassRequest calls are&amp;nbsp; made to SET_LINE_CODING. You could track the sequence to get as close to&amp;nbsp; the port being fully open, but I just watch for a SET_LINE_CODING call.&amp;nbsp; The port is actually opened and working a short time later. That's the not so perfect part, the amount of time before the port is actually opened varies depending on the speed of the host computer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Two things occur that indicate a port closing. First, in the HandleClassRequest function if you get two consecutive calls with&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SET_CONTROL_LINE_STATE&amp;nbsp; 0 that indicates the host computer closed the port gracefully. Second,&amp;nbsp; if you get a device status interrupt call to USBHwISR and devStatus ==&amp;nbsp; 13 the port hardware was disconnected, ie usb plug pulled abruptly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I added a function that just returns vcom_portOpen that can be called to see if the port is open.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;HandleClassRequest function with mods...&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
static BOOL HandleClassRequest(TSetupPacket *pSetup, int *piLen, U8 **ppbData)
{
&amp;nbsp;&amp;nbsp;&amp;nbsp; static uint8_t setStateCnt = 0; // jjsd: keep track of consecutive SET_CONTROL_LINE_STATE 0 calls

&amp;nbsp;&amp;nbsp;&amp;nbsp; switch (pSetup-&amp;gt;bRequest)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {

&amp;nbsp;&amp;nbsp;&amp;nbsp; // set line coding
&amp;nbsp;&amp;nbsp;&amp;nbsp; case SET_LINE_CODING:
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DBG("SET_LINE_CODING\r\n");
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; memcpy((U8 *) &amp;amp;LineCoding, *ppbData, 7);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *piLen = 7;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DBG("dwDTERate=%u, bCharFormat=%u, bParityType=%u, bDataBits=%u\r\n",
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LineCoding.dwDTERate,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LineCoding.bCharFormat,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LineCoding.bParityType,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LineCoding.bDataBits);

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; setStateCnt = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: reset our consecutive SET_CONTROL_LINE_STATE 0 count
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vcom_portOpen = TRUE;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: indicate the port is open
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // get line coding
&amp;nbsp;&amp;nbsp;&amp;nbsp; case GET_LINE_CODING:
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DBG("GET_LINE_CODING\r\n");
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ppbData = (U8 *) &amp;amp;LineCoding;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *piLen = 7;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; setStateCnt = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: reset our consecutive SET_CONTROL_LINE_STATE 0 count
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // set control line state
&amp;nbsp;&amp;nbsp;&amp;nbsp; case SET_CONTROL_LINE_STATE:
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // bit0 = DTR, bit = RTS
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DBG("SET_CONTROL_LINE_STATE %X\r\n", pSetup-&amp;gt;wValue);

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (pSetup-&amp;gt;wValue == 0)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: keep track of SET_CONTROL_LINE_STATE 0 consecutive count
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; setStateCnt++;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (setStateCnt == 2)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: two consecutive SET_CONTROL_LINE_STATE 0 means the port is closing
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vcom_portOpen = FALSE;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: indicate the port is closed
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;

&amp;nbsp;&amp;nbsp;&amp;nbsp; default:
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return FALSE;
&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; return TRUE;
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;USBHwISR function with mods...&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;void USBHwISR(void)
{
&amp;nbsp;&amp;nbsp;&amp;nbsp; U32 dwStatus;
&amp;nbsp;&amp;nbsp;&amp;nbsp; U32 dwIntBit;
&amp;nbsp;&amp;nbsp;&amp;nbsp; U8 bEPStat, bDevStat, bStat;
&amp;nbsp;&amp;nbsp;&amp;nbsp; int i;
&amp;nbsp;&amp;nbsp;&amp;nbsp; U16 wFrame;

&amp;nbsp;&amp;nbsp;&amp;nbsp; // LED9 monitors total time in interrupt routine
&amp;nbsp;&amp;nbsp;&amp;nbsp; DEBUG_LED_ON(6);

&amp;nbsp;&amp;nbsp;&amp;nbsp; // handle device interrupts
&amp;nbsp;&amp;nbsp;&amp;nbsp; dwStatus = LPC_USB-&amp;gt;USBDevIntSt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; // frame interrupt
&amp;nbsp;&amp;nbsp;&amp;nbsp; if (dwStatus &amp;amp; FRAME)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clear int
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_USB-&amp;gt;USBDevIntClr = FRAME;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // call handler
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (_pfnFrameHandler != NULL)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wFrame = USBHwCmdRead(CMD_DEV_READ_CUR_FRAME_NR);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _pfnFrameHandler(wFrame);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; }

&amp;nbsp;&amp;nbsp;&amp;nbsp; // device status interrupt
&amp;nbsp;&amp;nbsp;&amp;nbsp; if (dwStatus &amp;amp; DEV_STAT)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*&amp;nbsp;&amp;nbsp;&amp;nbsp; Clear DEV_STAT interrupt before reading DEV_STAT register.
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This prevents corrupted device status reads, see
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC2148 User manual revision 2, 25 july 2006.
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_USB-&amp;gt;USBDevIntClr = DEV_STAT;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bDevStat = USBHwCmdRead(CMD_DEV_STATUS);

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (bDevStat == 13)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: bDevStat == 13 indicates the usb hardware has been disconnected
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; vcom_portOpen = FALSE;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // jjsd: indicate port is closed

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (bDevStat &amp;amp; (CON_CH | SUS_CH | RST))
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // convert device status into something HW independent
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bStat = ((bDevStat &amp;amp; CON) ? DEV_STATUS_CONNECT : 0) | ((bDevStat &amp;amp; SUS) ? DEV_STATUS_SUSPEND : 0)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | ((bDevStat &amp;amp; RST) ? DEV_STATUS_RESET : 0);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // call handler
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (_pfnDevIntHandler != NULL)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEBUG_LED_ON(5);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _pfnDevIntHandler(bStat);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEBUG_LED_OFF(5);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; }

&amp;nbsp;&amp;nbsp;&amp;nbsp; // endpoint interrupt
&amp;nbsp;&amp;nbsp;&amp;nbsp; if (dwStatus &amp;amp; EP_SLOW)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clear EP_SLOW
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_USB-&amp;gt;USBDevIntClr = EP_SLOW;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // check all endpoints
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (i = 0; i &amp;lt; 32; i++)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dwIntBit = (1 &amp;lt;&amp;lt; i);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (LPC_USB-&amp;gt;USBEpIntSt &amp;amp; dwIntBit)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clear int (and retrieve status)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_USB-&amp;gt;USBEpIntClr = dwIntBit;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wait4DevInt(CDFULL);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bEPStat = LPC_USB-&amp;gt;USBCmdData;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // convert EP pipe stat into something HW independent
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bStat = ((bEPStat &amp;amp; EPSTAT_FE) ? EP_STATUS_DATA : 0) | ((bEPStat &amp;amp; EPSTAT_ST) ? EP_STATUS_STALLED : 0)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | ((bEPStat &amp;amp; EPSTAT_STP) ? EP_STATUS_SETUP : 0) | ((bEPStat &amp;amp; EPSTAT_EPN) ? EP_STATUS_NACKED
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 0) | ((bEPStat &amp;amp; EPSTAT_PO) ? EP_STATUS_ERROR : 0);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // call handler
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (_apfnEPIntHandlers[i / 2] != NULL)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEBUG_LED_ON(7);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _apfnEPIntHandlers[i / 2](IDX2EP(i), bStat);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEBUG_LED_OFF(7);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; }

&amp;nbsp;&amp;nbsp;&amp;nbsp; DEBUG_LED_OFF(6);
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/detecting-usb-attachment/m-p/564986#M17824</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:21:45Z</dc:date>
    </item>
  </channel>
</rss>