<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックFlash-Tool in GUI locks up on Mac</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Tool-in-GUI-locks-up-on-Mac/m-p/564759#M17723</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sravet on Thu Jan 03 21:01:06 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using FlashTool (the chip icon in the GUI) to download .bin and .axf files to both an LPCxpresso LPC1114 board and to a custom board with LPC1768.&amp;nbsp; All of these have the same behavior:&amp;nbsp; I select the file, verify the proper CPU architecture, then click OK and am presented with a progress bar that never progresses.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;From the shell I am able to see the command that lpcxpresso uses to flash (crt_emu_lpc11_13_nxp or crt_emu_cm3_nxp), and if I run it manually from the shell then it seems to complete fine.&amp;nbsp; Not sure what the GUI is waiting on.&amp;nbsp; in the shell ps -ax shows that the the flash programmer is still running, although if I copy/paste the exact same command to the shell prompt it runs and exits fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCxpresso version is 5.0.14, and I am running on a Mac.&amp;nbsp; Any suggestions on how to further debug this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--steve&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:25:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:25:04Z</dc:date>
    <item>
      <title>Flash-Tool in GUI locks up on Mac</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Tool-in-GUI-locks-up-on-Mac/m-p/564759#M17723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sravet on Thu Jan 03 21:01:06 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using FlashTool (the chip icon in the GUI) to download .bin and .axf files to both an LPCxpresso LPC1114 board and to a custom board with LPC1768.&amp;nbsp; All of these have the same behavior:&amp;nbsp; I select the file, verify the proper CPU architecture, then click OK and am presented with a progress bar that never progresses.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;From the shell I am able to see the command that lpcxpresso uses to flash (crt_emu_lpc11_13_nxp or crt_emu_cm3_nxp), and if I run it manually from the shell then it seems to complete fine.&amp;nbsp; Not sure what the GUI is waiting on.&amp;nbsp; in the shell ps -ax shows that the the flash programmer is still running, although if I copy/paste the exact same command to the shell prompt it runs and exits fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCxpresso version is 5.0.14, and I am running on a Mac.&amp;nbsp; Any suggestions on how to further debug this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--steve&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Tool-in-GUI-locks-up-on-Mac/m-p/564759#M17723</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:25:04Z</dc:date>
    </item>
  </channel>
</rss>