<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックFlash Programming binaries</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Programming-binaries/m-p/564333#M17526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JoeMoney on Fri Apr 23 17:38:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When I debug the program, it run fines on the lpc1114 board. But when i tried to directly program the binary using "Program Flash..." from the Binary Utilities, it doesn't run as it suppose to like its waiting for the run command... are there additional steps to the lpc1114 board when using Program Flash to make the program run?&lt;/SPAN&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338231"&gt;1100328_blinky_main.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:17:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:17:07Z</dc:date>
    <item>
      <title>Flash Programming binaries</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Programming-binaries/m-p/564333#M17526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JoeMoney on Fri Apr 23 17:38:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When I debug the program, it run fines on the lpc1114 board. But when i tried to directly program the binary using "Program Flash..." from the Binary Utilities, it doesn't run as it suppose to like its waiting for the run command... are there additional steps to the lpc1114 board when using Program Flash to make the program run?&lt;/SPAN&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338231"&gt;1100328_blinky_main.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Programming-binaries/m-p/564333#M17526</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming binaries</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Programming-binaries/m-p/564334#M17527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Sat Apr 24 09:37:03 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;After programming the flash, the utility leaves the target halted. If you reset or power cycle the device then it will start running the code you have programmed.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Flash-Programming-binaries/m-p/564334#M17527</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:17:08Z</dc:date>
    </item>
  </channel>
</rss>