<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC Xpresso Target 1769 - Example Code - Command line verification</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Xpresso-Target-1769-Example-Code-Command-line-verification/m-p/563787#M17272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Cheesyc on Tue Apr 16 14:24:13 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to verify that my command line flash is functioning correctly. I am looking for:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Code that was previously installed on the LPCXpresso board so I can load the code and see the LED blink (verification that my code went throught)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Example code I can load into the LPCXpresso that blinks the LED.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have attached a copy of my command line (:(I loaded a random file to see if it will load, which is why I need original file or LED blinker)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know how long it takes for the computer to recognize the debugger before I can use "bootlpcxpresso.cmd hid" ? I had an issue where it did not want to take but after a while, it seemed to start working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions would be great. Thanks!:rolleyes:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:54:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:54:23Z</dc:date>
    <item>
      <title>LPC Xpresso Target 1769 - Example Code - Command line verification</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Xpresso-Target-1769-Example-Code-Command-line-verification/m-p/563787#M17272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Cheesyc on Tue Apr 16 14:24:13 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to verify that my command line flash is functioning correctly. I am looking for:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Code that was previously installed on the LPCXpresso board so I can load the code and see the LED blink (verification that my code went throught)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Example code I can load into the LPCXpresso that blinks the LED.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have attached a copy of my command line (:(I loaded a random file to see if it will load, which is why I need original file or LED blinker)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know how long it takes for the computer to recognize the debugger before I can use "bootlpcxpresso.cmd hid" ? I had an issue where it did not want to take but after a while, it seemed to start working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any suggestions would be great. Thanks!:rolleyes:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:54:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Xpresso-Target-1769-Example-Code-Command-line-verification/m-p/563787#M17272</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:54:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC Xpresso Target 1769 - Example Code - Command line verification</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Xpresso-Target-1769-Example-Code-Command-line-verification/m-p/563788#M17273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Tue Apr 16 23:47:41 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There are lots of examples provided, including various "blinky" applications. Read the Getting Started for information on how to import/build/debug the examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The very first time you connect and LPC-Link to your PC, it ill take Windows several seconds to recognise the device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The first time you connect LPC-Link after a boot, Windows will take up to a couple of seconds to locate the driver. Afterwards, it will take less than a second.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The actual time depends on speed of your PC and how many other device drivers you have installed.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-Xpresso-Target-1769-Example-Code-Command-line-verification/m-p/563788#M17273</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:54:24Z</dc:date>
    </item>
  </channel>
</rss>