<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 multiple lpc-link at the same time</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563448#M17130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Chrysaor on Mon Jul 07 04:14:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have got a problem using multiple lpc-links at the same time. It is not possible to choose which of them (same vendor and device id) should boot at first.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When trying to use dfu-util -p only "USB device paths are not supported by this dfu-util." appears. Has someone already tried to use multiple lpc-links at the same time? We have to use up to eight of them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:40:55 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:40:55Z</dc:date>
    <item>
      <title>multiple lpc-link at the same time</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563448#M17130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Chrysaor on Mon Jul 07 04:14:46 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have got a problem using multiple lpc-links at the same time. It is not possible to choose which of them (same vendor and device id) should boot at first.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When trying to use dfu-util -p only "USB device paths are not supported by this dfu-util." appears. Has someone already tried to use multiple lpc-links at the same time? We have to use up to eight of them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563448#M17130</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: multiple lpc-link at the same time</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563449#M17131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Mon Jul 07 05:14:33 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You should be able connect and debug as many LPC-Links as you want, but you should be aware that it is not possible to uniquely identify an individual LPC-Link. Therefore, you will need to connect each board and launch a debug session before connecting the next LPC-Link.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Out of interest, what are you actually doing ?? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563449#M17131</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: multiple lpc-link at the same time</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563450#M17132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Chrysaor on Mon Jul 07 08:10:01 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;We want to build up a test bench for up to eight individual circuits which should perform a test of the circuitry after production. The idea was to use for that individual lpc-links connected to the pcbs, to perform the testing process. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to change the usb device id inside the LPCXpressoWIN.enc file to distinguish between the different boards?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you have another idea to do this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Christian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/multiple-lpc-link-at-the-same-time/m-p/563450#M17132</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:40:57Z</dc:date>
    </item>
  </channel>
</rss>