<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to communicate between two lpc1769 board using ethernet(EMAC) in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563390#M17105</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sun Jul 31 23:22:31 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In that case I would suggest to start from the EasyWeb example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With the LPCXpresso 4.0.5 tools this can be found in NXP\LPC1000\LPC17xx\LPCXpresso176x_cmsis2.zip.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The ethmac.c in this example supports both the DP83848 (found on the MBC1700 and RDB1768 boards) and the 7820 found on the LPCXpresso board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The EMAC example found in the MBC1700 examples projects only supports the DP83848 phy chip so that is not a good point to start from.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As soon as you get that running you have a stable base to start from (at least then you know the basic initializations and communications do work).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:19:05 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:19:05Z</dc:date>
    <item>
      <title>How to communicate between two lpc1769 board using ethernet(EMAC)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563386#M17101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aarthi on Fri Jul 29 22:25:01 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Now i am working with lpc1769 microcontroller. I just need to know how to communicate between two lpc1769 boards using EMAC. I also tried the EMAC example which is given the IDE but i am not able to communicate and also the code was really tuff to understand .so can anyone help me how to work in this ethernet.:confused:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563386#M17101</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: How to communicate between two lpc1769 board using ethernet(EMAC)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563387#M17102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Europe on Sat Jul 30 15:35:17 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello aarthi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;did you check on the NXP-website for example code?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;see: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/?search=ethernet&amp;amp;locale=en%2C%2CLatn&amp;amp;type=appnote&amp;amp;sort=date&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563387#M17102</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to communicate between two lpc1769 board using ethernet(EMAC)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563388#M17103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sat Jul 30 23:04:48 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It would be good if aarthi could provide some more info.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What kind of boards are you using?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With "communicating between 2 boards with EMAC" do you mean that you connect two boards via a normal ethernet connection (e.g. using the LAN8720A chip on the LPCXpresso board) or are you trying to connect two chips directly using the MAC interface (using the P0.x pins directly) ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563388#M17103</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: How to communicate between two lpc1769 board using ethernet(EMAC)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563389#M17104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aarthi on Sun Jul 31 20:42:37 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to connect two boards via normal ethernet connection (using the LAN 8720A on the LPC XPRESSO Board)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563389#M17104</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:19:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to communicate between two lpc1769 board using ethernet(EMAC)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563390#M17105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Sun Jul 31 23:22:31 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In that case I would suggest to start from the EasyWeb example.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With the LPCXpresso 4.0.5 tools this can be found in NXP\LPC1000\LPC17xx\LPCXpresso176x_cmsis2.zip.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The ethmac.c in this example supports both the DP83848 (found on the MBC1700 and RDB1768 boards) and the 7820 found on the LPCXpresso board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The EMAC example found in the MBC1700 examples projects only supports the DP83848 phy chip so that is not a good point to start from.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As soon as you get that running you have a stable base to start from (at least then you know the basic initializations and communications do work).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-to-communicate-between-two-lpc1769-board-using-ethernet-EMAC/m-p/563390#M17105</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:19:05Z</dc:date>
    </item>
  </channel>
</rss>