<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Getting the clock signal</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529860#M1689</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by renan on Wed Sep 22 11:44:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is the LPCXpresso forum. :D&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Renan&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:03:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:03:42Z</dc:date>
    <item>
      <title>Getting the clock signal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529859#M1688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by shobley on Wed Sep 22 11:39:25 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm currently experimenting with the LPCXpresso board, but since they did not have a support forum, I thought I would post my question here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know if I can access the 12Mhz clock signal and use it to drive another device (Pixart sensor)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Or is there a way to generate an 8-12Mhz clock signal from one of the pins without too much load. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ideally I would just like to tap the built in crystal, but using some kind of PWM has been known to work with the Atmel AVR chips.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help greatly appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Steve&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529859#M1688</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: Getting the clock signal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529860#M1689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by renan on Wed Sep 22 11:44:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is the LPCXpresso forum. :D&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Renan&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529860#M1689</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: Getting the clock signal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529861#M1690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Jesse.Rosenberg on Wed Sep 22 12:35:01 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The clock output pin is primarily intended for diagnostic purposes, rather than for clock synthesis. Using a divider value of 2, for instance, can be used to observe an internal 100MHz clock frequency using lower end lab equipment, such as a USB based oscilloscope with limited bandwidth.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You should bear in mind that should your design make use of in system programming (ISP) via the chip's boot loader for software updates, you'll most likely be using P0_1, which is typically a clock output pin.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Getting-the-clock-signal/m-p/529861#M1690</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:03:42Z</dc:date>
    </item>
  </channel>
</rss>