<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックSPI communucation with external ADC</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-communucation-with-external-ADC/m-p/562652#M16844</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drizzt on Tue Mar 15 08:47:27 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to connect external ACD, AD7680 and LPC1343with SPI line &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;in examples of SPI, there is only examples of Master send and Slave receive, but I need Master to receive&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;with current configuration, I think that clock is 0.5MHz, can someone confirm this ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;AD7680 sends 24bits, of that 16 bits of information&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;my intention was to set FIFO frames to 4-bit transfer, and from 4 frames get information&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;problem is that in current code, I don't get anything on line SCK when viewing on digital oscilloscope&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;help, please!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;at least point me to some web places where to find some information&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thnx in advance&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:13:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:13:01Z</dc:date>
    <item>
      <title>SPI communucation with external ADC</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-communucation-with-external-ADC/m-p/562652#M16844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by drizzt on Tue Mar 15 08:47:27 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to connect external ACD, AD7680 and LPC1343with SPI line &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;in examples of SPI, there is only examples of Master send and Slave receive, but I need Master to receive&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;with current configuration, I think that clock is 0.5MHz, can someone confirm this ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;AD7680 sends 24bits, of that 16 bits of information&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;my intention was to set FIFO frames to 4-bit transfer, and from 4 frames get information&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;problem is that in current code, I don't get anything on line SCK when viewing on digital oscilloscope&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;help, please!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;at least point me to some web places where to find some information&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thnx in advance&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-communucation-with-external-ADC/m-p/562652#M16844</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:13:01Z</dc:date>
    </item>
  </channel>
</rss>