<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 LPCXpresso and LPCScrypt current status using Mac OSX 10.11 El Capitan</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562033#M16558</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 02:00:43 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[h1]Update : 23rd February 2016[/h1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the release of LPCXpresso IDE v8.1.0, the remaining Mac OS X 10.11 El Capitan issue - the failure of LPC-Link1 probes to boot - has now been resolved. The use of Mac OS X 10.11.3 or later is recommended.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[h1]Older information[/h1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;General LPCXpresso IDE behaviour running under Mac OSX 10.11 El Capitan is as per using Yosemite. And LPC-Link2 debug probes with CMSIS-DAP firmware operate without problems including the LPC-Link2 probes built into LPCXpresso V2/V3 boards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, we are currently investigating a number of USB related issues detailed below. The LPCXpresso team is actively working to address these issues and will post further information when it becomes available. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; [size=20]&lt;/SPAN&gt;&lt;STRONG&gt;[u]LPC-Link1 probes fail to boot:[/u]&lt;/STRONG&gt;&lt;SPAN&gt;[/size]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In fact, the LPC-Link1 probe does boot, however the OS fails to recognize and re-enumerate the new device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To work around this problem you can:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[list=1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]connect the Link1 probe to the Mac via a powered hub.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]use the GUI icon or Command line script to boot the probe&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]disconnect the hub from the Mac for a second or so and reconnect&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The booted LPC-Link1 will now appear and can be used to debug as usual. Provided power is maintained to the LPC-Link1 device, the soft loaded firmware will continue to run.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fbooting-lpc-link" rel="nofollow noopener noreferrer" target="_blank"&gt;https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; [size=20]&lt;/SPAN&gt;&lt;STRONG&gt;[u]Red Probe+ is not recognized by the LPCXpresso IDE[/u]&lt;/STRONG&gt;&lt;SPAN&gt;[/size]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently we have no work around for this problem, and we would recommend that you consider switching to using an LPC-Link2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;*UPDATE*&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the lastest release of OSX El Capitan (currently 10.11.2), this problem has been addressed and Red Probe+ works as before. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; [size=20]&lt;/SPAN&gt;&lt;STRONG&gt;[u]LPCScrypt fails some operations[/u]&lt;/STRONG&gt;&lt;SPAN&gt;[/size]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;*UPDATE*&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The latest release of LPCScrypt v1.6.0 now works out of the box with OSX El Capitan.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In versions of LPCScrypt prior to v1.6.0:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPCScrypt bulk data transfer mechanism is failing on the host side leading to errors of the form:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;LPC_Error dataBurst Timeout 0xe 0xc8
Error: &amp;lt;Command line&amp;gt;:1: dataBurst Timeout 0xe 0xc8
&amp;nbsp;&amp;nbsp; Script cmd:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; program …..
&amp;nbsp;&amp;nbsp; Last target cmd: =databurst …..
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This will impact operations that transfer larger quantities of data such as program and verify. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To workaround for this problem you can reduce the size of bulk transfer operations using the -m switch, where 200 is the maximum safe value. For example:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;bin/lpcscrypt -m 200 program path_to_bin SPIFI &lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note however that scripts provided within LPCScrypt such as programCMSIS and programJLINK will also exhibit this problem. These scripts can be manually edited as described above. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note also that on Mac's, LPCScrypt automatically installs into the Applications directory. Editing files within this directory required Administrator privilege.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:51:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:51:23Z</dc:date>
    <item>
      <title>LPCXpresso and LPCScrypt current status using Mac OSX 10.11 El Capitan</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562033#M16558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 02:00:43 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[h1]Update : 23rd February 2016[/h1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;With the release of LPCXpresso IDE v8.1.0, the remaining Mac OS X 10.11 El Capitan issue - the failure of LPC-Link1 probes to boot - has now been resolved. The use of Mac OS X 10.11.3 or later is recommended.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[h1]Older information[/h1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;General LPCXpresso IDE behaviour running under Mac OSX 10.11 El Capitan is as per using Yosemite. And LPC-Link2 debug probes with CMSIS-DAP firmware operate without problems including the LPC-Link2 probes built into LPCXpresso V2/V3 boards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, we are currently investigating a number of USB related issues detailed below. The LPCXpresso team is actively working to address these issues and will post further information when it becomes available. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; [size=20]&lt;/SPAN&gt;&lt;STRONG&gt;[u]LPC-Link1 probes fail to boot:[/u]&lt;/STRONG&gt;&lt;SPAN&gt;[/size]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In fact, the LPC-Link1 probe does boot, however the OS fails to recognize and re-enumerate the new device.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To work around this problem you can:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[list=1]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]connect the Link1 probe to the Mac via a powered hub.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]use the GUI icon or Command line script to boot the probe&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]disconnect the hub from the Mac for a second or so and reconnect&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The booted LPC-Link1 will now appear and can be used to debug as usual. Provided power is maintained to the LPC-Link1 device, the soft loaded firmware will continue to run.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fbooting-lpc-link" rel="nofollow noopener noreferrer" target="_blank"&gt;https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; [size=20]&lt;/SPAN&gt;&lt;STRONG&gt;[u]Red Probe+ is not recognized by the LPCXpresso IDE[/u]&lt;/STRONG&gt;&lt;SPAN&gt;[/size]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently we have no work around for this problem, and we would recommend that you consider switching to using an LPC-Link2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;*UPDATE*&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the lastest release of OSX El Capitan (currently 10.11.2), this problem has been addressed and Red Probe+ works as before. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; [size=20]&lt;/SPAN&gt;&lt;STRONG&gt;[u]LPCScrypt fails some operations[/u]&lt;/STRONG&gt;&lt;SPAN&gt;[/size]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;*UPDATE*&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The latest release of LPCScrypt v1.6.0 now works out of the box with OSX El Capitan.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In versions of LPCScrypt prior to v1.6.0:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPCScrypt bulk data transfer mechanism is failing on the host side leading to errors of the form:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;LPC_Error dataBurst Timeout 0xe 0xc8
Error: &amp;lt;Command line&amp;gt;:1: dataBurst Timeout 0xe 0xc8
&amp;nbsp;&amp;nbsp; Script cmd:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; program …..
&amp;nbsp;&amp;nbsp; Last target cmd: =databurst …..
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This will impact operations that transfer larger quantities of data such as program and verify. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To workaround for this problem you can reduce the size of bulk transfer operations using the -m switch, where 200 is the maximum safe value. For example:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;bin/lpcscrypt -m 200 program path_to_bin SPIFI &lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note however that scripts provided within LPCScrypt such as programCMSIS and programJLINK will also exhibit this problem. These scripts can be manually edited as described above. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note also that on Mac's, LPCScrypt automatically installs into the Applications directory. Editing files within this directory required Administrator privilege.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562033#M16558</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:51:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso and LPCScrypt current status using Mac OSX 10.11 El Capitan</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562034#M16559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Thu Nov 05 08:47:58 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Updated Red Probe+ information (fixed in latest El Capitan 10.11.2 beta)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:51:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562034#M16559</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:51:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso and LPCScrypt current status using Mac OSX 10.11 El Capitan</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562035#M16560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 02:02:27 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With the release of LPCXpresso IDE v8.1.0, the remaining Mac OS X 10.11 El Capitan issue - the failure of LPC-Link1 probes to boot - has now been resolved. The use of Mac OS X 10.11.3 or later is recommended.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-LPCScrypt-current-status-using-Mac-OSX-10-11-El/m-p/562035#M16560</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:51:24Z</dc:date>
    </item>
  </channel>
</rss>