<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Internal Pull- ups in SPI protocol, LPC1317-64P</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Internal-Pull-ups-in-SPI-protocol-LPC1317-64P/m-p/561898#M16503</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leon_heller on Mon Mar 04 04:47:50 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Pull-ups aren't required for SPI.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:40:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:40:26Z</dc:date>
    <item>
      <title>Internal Pull- ups in SPI protocol, LPC1317-64P</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Internal-Pull-ups-in-SPI-protocol-LPC1317-64P/m-p/561897#M16502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by aamir ali on Mon Mar 04 00:07:47 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;1 .Since in MISO0 line is input pin, so is there need of using internal pull up of LPC1317, so avoid floating condition.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Or we can put pull up at both MISO &amp;amp; MOSI lines without problem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If yes,MOSI is output pin so on having internal pull up enabled is right, or it will affect the circuit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Or I should not use pull up with any of line.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have interface SD card with SPI protocol&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Internal-Pull-ups-in-SPI-protocol-LPC1317-64P/m-p/561897#M16502</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Pull- ups in SPI protocol, LPC1317-64P</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Internal-Pull-ups-in-SPI-protocol-LPC1317-64P/m-p/561898#M16503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leon_heller on Mon Mar 04 04:47:50 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Pull-ups aren't required for SPI.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:40:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Internal-Pull-ups-in-SPI-protocol-LPC1317-64P/m-p/561898#M16503</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:40:26Z</dc:date>
    </item>
  </channel>
</rss>