<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1788 Embedded Artists LCD. in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1788-Embedded-Artists-LCD/m-p/529714#M1640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by btuline on Fri Jun 28 16:59:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hey I'm really new to the LPC1788, and I'm trying to get the LCD working through an example program. The code I'm trying to upload is the emWin board support package sample program found here: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.lpcware.com/content/project/emwin-graphics-library&lt;/A&gt;&lt;SPAN&gt;. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The only changes I've made to the example is a modification to the project file output in order to generate a hex file to upload using Flash Magic. The instructions I followed to set that up were found here: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/OutputFormats&lt;/A&gt;&lt;SPAN&gt;, and I've tried setting it up to add a check sum in Flash Magic and LPCXpresso with those instructions. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now the problem I'm having is that loading the program successfully completes in Flash Magic. However there is not ouput being shown on the LCD other than the backlight. and I have no idea why this would happen with the sample program. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyone have any suggestions for what I could have missed? And if theres anything important I might have left out let me know.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:33:45 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:33:45Z</dc:date>
    <item>
      <title>LPC1788 Embedded Artists LCD.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1788-Embedded-Artists-LCD/m-p/529714#M1640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by btuline on Fri Jun 28 16:59:14 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hey I'm really new to the LPC1788, and I'm trying to get the LCD working through an example program. The code I'm trying to upload is the emWin board support package sample program found here: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.lpcware.com/content/project/emwin-graphics-library&lt;/A&gt;&lt;SPAN&gt;. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The only changes I've made to the example is a modification to the project file output in order to generate a hex file to upload using Flash Magic. The instructions I followed to set that up were found here: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/OutputFormats&lt;/A&gt;&lt;SPAN&gt;, and I've tried setting it up to add a check sum in Flash Magic and LPCXpresso with those instructions. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now the problem I'm having is that loading the program successfully completes in Flash Magic. However there is not ouput being shown on the LCD other than the backlight. and I have no idea why this would happen with the sample program. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyone have any suggestions for what I could have missed? And if theres anything important I might have left out let me know.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1788-Embedded-Artists-LCD/m-p/529714#M1640</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:33:45Z</dc:date>
    </item>
  </channel>
</rss>