<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC 122x  ROM Bootloader  using UART0</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-122x-ROM-Bootloader-using-UART0/m-p/561354#M16283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by spongehead on Wed Feb 20 17:58:16 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;On reset of LPCExpresso 122x (using LPC1227 module), if the ROM bootloader using UART0 is invoked,&amp;nbsp; does the bootloader code set the IOCONFIG&amp;nbsp; for PIO0_1 to be RXD0 and PIO0_2 to be TXD0?&amp;nbsp;&amp;nbsp; Is there a way to change this without changing the bootloader code itself to use the alternate PIO2_1 (RXD0) and PIO2_2 (TXD0) pins for UART0?&amp;nbsp;&amp;nbsp; Just started on using th LPC1227 module, so any input is appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:37:14 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:37:14Z</dc:date>
    <item>
      <title>LPC 122x  ROM Bootloader  using UART0</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-122x-ROM-Bootloader-using-UART0/m-p/561354#M16283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by spongehead on Wed Feb 20 17:58:16 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;On reset of LPCExpresso 122x (using LPC1227 module), if the ROM bootloader using UART0 is invoked,&amp;nbsp; does the bootloader code set the IOCONFIG&amp;nbsp; for PIO0_1 to be RXD0 and PIO0_2 to be TXD0?&amp;nbsp;&amp;nbsp; Is there a way to change this without changing the bootloader code itself to use the alternate PIO2_1 (RXD0) and PIO2_2 (TXD0) pins for UART0?&amp;nbsp;&amp;nbsp; Just started on using th LPC1227 module, so any input is appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-122x-ROM-Bootloader-using-UART0/m-p/561354#M16283</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 122x  ROM Bootloader  using UART0</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-122x-ROM-Bootloader-using-UART0/m-p/561355#M16284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Feb 20 18:21:55 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You're right :) If you want different UART0 pins for ROM bootloader you've to ask NXP for your own LPC122x edition :cool:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC-122x-ROM-Bootloader-using-UART0/m-p/561355#M16284</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:15Z</dc:date>
    </item>
  </channel>
</rss>