<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic variable not refeshed or updated sync (without build) in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/variable-not-refeshed-or-updated-sync-without-build/m-p/561267#M16256</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by riscy00 on Sun Jan 26 04:28:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When I add new variable name within enum, typedef struct or just variable and so on (I call it symbol). I inserted variable/symbol in elsewhere but does not change to blue nor recognised, nor include symbol in the list (when hover on above symbol).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Most complier has automatic refresh or updated when new symbol is added. This IDE does not. To get it updated I had to rebuild which is not ideal way to do this because I have not finish coding and would generate complier error (and stop processing code/update symbol table?). &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I looked into "update", "refresh" in help but did not gave any correct answer that make sense.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;below is an example &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ALPS_NAV_OP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ALPS_NAV_OP.RotaryState=ALPS_Neutral;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had to manually insert RotaryState and ALPS_Neutral symbol after change within enum and typedef struct in header filename or other code filename because the symbol table is not updated. It is annoying to type manually. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;R.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:39:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:39:18Z</dc:date>
    <item>
      <title>variable not refeshed or updated sync (without build)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/variable-not-refeshed-or-updated-sync-without-build/m-p/561267#M16256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by riscy00 on Sun Jan 26 04:28:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When I add new variable name within enum, typedef struct or just variable and so on (I call it symbol). I inserted variable/symbol in elsewhere but does not change to blue nor recognised, nor include symbol in the list (when hover on above symbol).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Most complier has automatic refresh or updated when new symbol is added. This IDE does not. To get it updated I had to rebuild which is not ideal way to do this because I have not finish coding and would generate complier error (and stop processing code/update symbol table?). &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I looked into "update", "refresh" in help but did not gave any correct answer that make sense.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;below is an example &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ALPS_NAV_OP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ALPS_NAV_OP.RotaryState=ALPS_Neutral;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I had to manually insert RotaryState and ALPS_Neutral symbol after change within enum and typedef struct in header filename or other code filename because the symbol table is not updated. It is annoying to type manually. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;R.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/variable-not-refeshed-or-updated-sync-without-build/m-p/561267#M16256</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:39:18Z</dc:date>
    </item>
    <item>
      <title>Re: variable not refeshed or updated sync (without build)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/variable-not-refeshed-or-updated-sync-without-build/m-p/561268#M16257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sun Jan 26 05:11:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Try saving the file - that should cause the indexer to refresh. If not, right-click on the project and select Index-&amp;gt;Rebuild.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/variable-not-refeshed-or-updated-sync-without-build/m-p/561268#M16257</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:39:18Z</dc:date>
    </item>
  </channel>
</rss>