<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 SYGSYS:Bad System Call in __write()</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561114#M16171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by djlegge on Fri Aug 23 03:00:00 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi I am using LPCXpresso 5.2.6 in linux (Ubuntu 12.04) and have found what I think to be a small bug (or limitation) in the semihosting support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am debugging application code which is (in debug configuration) approx 110kB in size (the 'text' segment given by arm-none-eabi-size).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a secondary boot loader, so my application code is loaded in to memory at 0x8000.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the semihosting printf() feature and it works well until __write() moves above 0x20000. At this point, the printf output is still shown but the debugging stops with the above error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the free (128kB limited) version of LPCXpresso. I suspect somehow this is to do with the 128kB debug limit for this licence ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas ? Thanks.&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:38:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:38:42Z</dc:date>
    <item>
      <title>SYGSYS:Bad System Call in __write()</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561114#M16171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by djlegge on Fri Aug 23 03:00:00 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi I am using LPCXpresso 5.2.6 in linux (Ubuntu 12.04) and have found what I think to be a small bug (or limitation) in the semihosting support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am debugging application code which is (in debug configuration) approx 110kB in size (the 'text' segment given by arm-none-eabi-size).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a secondary boot loader, so my application code is loaded in to memory at 0x8000.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the semihosting printf() feature and it works well until __write() moves above 0x20000. At this point, the printf output is still shown but the debugging stops with the above error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the free (128kB limited) version of LPCXpresso. I suspect somehow this is to do with the 128kB debug limit for this licence ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas ? Thanks.&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561114#M16171</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: SYGSYS:Bad System Call in __write()</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561115#M16172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Aug 23 03:05:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That is correct, this is caused by the 128k debug limit.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561115#M16172</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:38:43Z</dc:date>
    </item>
    <item>
      <title>Re: SYGSYS:Bad System Call in __write()</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561116#M16173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by djlegge on Fri Aug 23 03:30:06 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the quick reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had assumed the 128k limit was an actual code size limit, rather than to do with the 0x20000 boundary - especially as it gives no errors programming.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For now I'll remove my bootloader for debugging purposes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:38:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SYGSYS-Bad-System-Call-in-write/m-p/561116#M16173</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:38:44Z</dc:date>
    </item>
  </channel>
</rss>