<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Cannot connect Debugger to Optimised Code</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Cannot-connect-Debugger-to-Optimised-Code/m-p/561012#M16140</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ian Stroud on Tue Mar 15 09:51:17 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Using LPCXPRESSO 3.6 I have built an application with -O1 / -O2 compiler flags.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The code initially downloads OK and seems to run as expected. However if I subsequently disconnect the debugger, power cycle the target, and then attempt to re-attach the debugger it fails with a warning stating "03: Failed on chip setup: Em(12)....": &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ATTACH]350[/ATTACH]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This does not happen if non-optimised debug code is loaded on the target. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can work around this problem if I turn on the debugger option "Vector Catch" but this does not help colleagues who are trying to update code using the command line utilities.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:14:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:14:04Z</dc:date>
    <item>
      <title>Cannot connect Debugger to Optimised Code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Cannot-connect-Debugger-to-Optimised-Code/m-p/561012#M16140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ian Stroud on Tue Mar 15 09:51:17 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Using LPCXPRESSO 3.6 I have built an application with -O1 / -O2 compiler flags.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The code initially downloads OK and seems to run as expected. However if I subsequently disconnect the debugger, power cycle the target, and then attempt to re-attach the debugger it fails with a warning stating "03: Failed on chip setup: Em(12)....": &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ATTACH]350[/ATTACH]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This does not happen if non-optimised debug code is loaded on the target. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can work around this problem if I turn on the debugger option "Vector Catch" but this does not help colleagues who are trying to update code using the command line utilities.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Cannot-connect-Debugger-to-Optimised-Code/m-p/561012#M16140</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:14:04Z</dc:date>
    </item>
  </channel>
</rss>