<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: IDE 5.1.2 Can't Find LPC-Link</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560472#M15879</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Thu Feb 21 20:53:31 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=1]Thanks, that did it, although I did not copy over a launch config ; I created one via the 'bug' icon on the toolbar.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I do create a debug launch via the 'bug' icon, I can use it ok. BUT when I click debug in quick start, it totally&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ignores any I have set up and makes a new one -- with all the wrong defaults for me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Why is this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(a) How can I get in and configure *BEFORE* the quickstart debug configuration runs for the first time?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(b) Why have you hidden the debug launch files (burried somewhere in .metadata IIRC) instead of leaving&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;them in the project directory (where some would argue that they belong -- are ther included in a project export?)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(c) The defaults are not what I want -- ever. Is there a way of setting a [I]workplace[/I] default debug configuration&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;so that every time I add a project (or I have to delete a launch config) I don't have to turn of red trace,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;set no semi-hosting, select SWD, select no load, etc. etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:37:28 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:37:28Z</dc:date>
    <item>
      <title>IDE 5.1.2 Can't Find LPC-Link</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560468#M15875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Thu Feb 21 08:17:44 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=2]I have installed LPCXpresso 5.1.2 in parallel with 5.1.0 (WinXP Pro SP3)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have given it its own work space and a separate copy of a project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(Identical source/Makefile/Linker script, but a separate directory.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I imported the 'Makefile Project' (File/New/Project); Set the MCU 1778.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I attempt to debug, it can't find any emulators (debug adapters)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My usual ploy of unplugging the USB cable and re-inserting did not work.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Closing 5.1.2 and opening 5.1.0; debug works as usual (emulator found etc.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Was there something I should have done (that doesn't seem to be documented&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;anywhere) or is this an 'issue' with 5.1.2?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked with ProcessExplorer from SystemInternals, no 'starter' or 'crt-...' processes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(or another LPCXpresso) were hanging about from a previous run (of either IDE).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As I only use the IDE for debugging, this is a bit of a bugger. (Pun intended.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560468#M15875</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:25Z</dc:date>
    </item>
    <item>
      <title>Re: IDE 5.1.2 Can't Find LPC-Link</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560469#M15876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Thu Feb 21 09:04:21 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;5.1.12 works here - exactly the same as 5.1.0.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560469#M15876</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: IDE 5.1.2 Can't Find LPC-Link</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560470#M15877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Thu Feb 21 09:09:24 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Trebuchet MS][SIZE=2]&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: TheFallGuy&lt;/STRONG&gt;&lt;BR /&gt;5.1.12 works here - exactly the same as 5.1.0.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, any clues as to what I should have (or not) done?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I ran the installer, just the same way as all previous released, with all the same&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;options.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you have both installed when you made your statement?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560470#M15877</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:27Z</dc:date>
    </item>
    <item>
      <title>Re: IDE 5.1.2 Can't Find LPC-Link</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560471#M15878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu Feb 21 11:09:44 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: MikeSimmonds&lt;/STRONG&gt;&lt;BR /&gt;[FONT=Trebuchet MS][SIZE=2]&lt;BR /&gt;So, any clues as to what I should have (or not) done?&lt;BR /&gt;I ran the installer, just the same way as all previous released, with all the same&lt;BR /&gt;options.&lt;BR /&gt;&lt;BR /&gt;Did you have both installed when you made your statement?&lt;BR /&gt;&lt;BR /&gt;Mike&lt;BR /&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Delete/recreate your launch/debug configurations. You should be prompted to connect to any supported emulator found attached to your USB port(s). There's no interaction between multiple LPCXpresso installations on the same computer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560471#M15878</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: IDE 5.1.2 Can't Find LPC-Link</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560472#M15879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Thu Feb 21 20:53:31 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[FONT=Tahoma][SIZE=1]Thanks, that did it, although I did not copy over a launch config ; I created one via the 'bug' icon on the toolbar.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When I do create a debug launch via the 'bug' icon, I can use it ok. BUT when I click debug in quick start, it totally&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ignores any I have set up and makes a new one -- with all the wrong defaults for me.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Why is this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(a) How can I get in and configure *BEFORE* the quickstart debug configuration runs for the first time?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(b) Why have you hidden the debug launch files (burried somewhere in .metadata IIRC) instead of leaving&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;them in the project directory (where some would argue that they belong -- are ther included in a project export?)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(c) The defaults are not what I want -- ever. Is there a way of setting a [I]workplace[/I] default debug configuration&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;so that every time I add a project (or I have to delete a launch config) I don't have to turn of red trace,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;set no semi-hosting, select SWD, select no load, etc. etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560472#M15879</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: IDE 5.1.2 Can't Find LPC-Link</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560473#M15880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Feb 22 01:32:33 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;a. Right-click and choose Launch configurations-&amp;gt;Create and open new&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;b. If you create your own, you also need to select the Common tab and choose "Local file" to place the file in your project&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;c. The default options are good for 99.9% of customers. You are the 0.1%&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/IDE-5-1-2-Can-t-Find-LPC-Link/m-p/560473#M15880</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:37:29Z</dc:date>
    </item>
  </channel>
</rss>