<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: ROM emulation</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559536#M15487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Europe on Thu Aug 04 06:04:54 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Straw-hat,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC1343 has two types of ROM, the Flash :) and a piece of ROM not accessible for writing.. ROM -&amp;gt; Read only Memory..;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to create power profiles as the LPC1313 or LPC11xx has, you could use a part of the Flash for doing this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You then need to place your API to your selected piece of Flash, and run it from there.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kind regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:15:59 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:15:59Z</dc:date>
    <item>
      <title>ROM emulation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559535#M15486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by straw_hat on Wed Aug 03 22:19:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i just want to ask if it is possible to emulate the ROM. like in lpc1343, i want to implement the power profile API which uses the ROM but the LPC1343 I believe does not contain a ROM. How can I possibly implement the power profile API(Set_Power). Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559535#M15486</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: ROM emulation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559536#M15487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Europe on Thu Aug 04 06:04:54 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Straw-hat,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC1343 has two types of ROM, the Flash :) and a piece of ROM not accessible for writing.. ROM -&amp;gt; Read only Memory..;)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to create power profiles as the LPC1313 or LPC11xx has, you could use a part of the Flash for doing this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You then need to place your API to your selected piece of Flash, and run it from there.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kind regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559536#M15487</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: ROM emulation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559537#M15488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by straw_hat on Thu Aug 04 17:56:19 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi thank you for the information. So it is really possible to implement power profile in LPC1343?? If so, can you please give an idea how to accomplish it, because as i read the user manual (UM10375), it does not include the LPC1343. Thank you&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559537#M15488</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: ROM emulation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559538#M15489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ktownsend on Sun Aug 07 13:30:50 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: straw_hat&lt;/STRONG&gt;&lt;BR /&gt;hi thank you for the information. So it is really possible to implement power profile in LPC1343?? If so, can you please give an idea how to accomplish it, because as i read the user manual (UM10375), it does not include the LPC1343. Thank you&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think you misunderstood.&amp;nbsp; Power profiles are ONLY present in the LPC1100L chips and the 'L' version of the LPC1313.&amp;nbsp; If you want to do this yourself in the LPC1343, you will need to write your own power management code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You could possibly write a program to read the ROM from an LPC1313 and reverse engineer some of the logic, but that's obviously a fairly significant endeavour, and there are likely to be some registers that are only available or valid on the L series chips (that won't be valid on the earlier LPC1343).&amp;nbsp; Presumably there were also some HW changes to improve the power performance of these newer chips since the L series has different characteristics for things like the voltage on pins using internal pullups, etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The short answer is ... if you want power profiles from ROM, you need to use an 'L' series LPC1100 or LPC1313 chip.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559538#M15489</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:16:00Z</dc:date>
    </item>
    <item>
      <title>Re: ROM emulation</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559539#M15490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by straw_hat on Sun Aug 07 18:10:04 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks for the information. so it is not really possible to implement power profile in LPC1343??thankks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ROM-emulation/m-p/559539#M15490</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:16:00Z</dc:date>
    </item>
  </channel>
</rss>