<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Linker errors on system calls</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559175#M15344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mawg on Mon Dec 05 23:41:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I had a nice litle s/w only project which I built using Cygwin in Netbeans under Windows 7.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then I learened that I would be using an LPC 1700 board for development, so I D/Led the Espesso clipse IDE and dropped my existing code inte it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The only errors I am getting are to do with system calls, such as&amp;nbsp; ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
f:/dropbox/programs/lpcxpresso/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-exit.o): In function `exit':
exit.c:(.text+0x1c): undefined reference to `_exit'
f:/dropbox/programs/lpcxpresso/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-fstatr.o): In function `_fstat_r':&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;While I would epxect it to work right out of the box, I suspect that I need a #define somewhere.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any idea? I asure that this is a stoopid n00b error, but I can't find an answer by googling.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for any help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:49:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:49:23Z</dc:date>
    <item>
      <title>Linker errors on system calls</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559175#M15344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mawg on Mon Dec 05 23:41:45 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I had a nice litle s/w only project which I built using Cygwin in Netbeans under Windows 7.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then I learened that I would be using an LPC 1700 board for development, so I D/Led the Espesso clipse IDE and dropped my existing code inte it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The only errors I am getting are to do with system calls, such as&amp;nbsp; ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
f:/dropbox/programs/lpcxpresso/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-exit.o): In function `exit':
exit.c:(.text+0x1c): undefined reference to `_exit'
f:/dropbox/programs/lpcxpresso/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/lib/thumb2\libc.a(lib_a-fstatr.o): In function `_fstat_r':&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;While I would epxect it to work right out of the box, I suspect that I need a #define somewhere.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any idea? I asure that this is a stoopid n00b error, but I can't find an answer by googling.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for any help.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:49:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559175#M15344</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:49:23Z</dc:date>
    </item>
    <item>
      <title>Re: Linker errors on system calls</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559176#M15345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Tue Dec 06 01:49:00 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you see the FAQ:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/UndefinedReference&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;BTW: when running on an embedded system, it is really not a good idea to call exit - what do you think it is going to do?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559176#M15345</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:49:24Z</dc:date>
    </item>
    <item>
      <title>Re: Linker errors on system calls</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559177#M15346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mawg on Tue Dec 06 02:10:58 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks. Your link looks very useful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Exit() is only called on the host (#if TESTING==UNIT_TEST), it just happened to be the first error message. I presume that I am calling all of the others somehow and just need to configure things correctly (one fix should cure all). I am sure that your link will shed light on it. Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-errors-on-system-calls/m-p/559177#M15346</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:49:25Z</dc:date>
    </item>
  </channel>
</rss>