<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1769 as USB Host Controller for CDC in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-as-USB-Host-Controller-for-CDC/m-p/559124#M15321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by muamw10 on Wed Feb 29 13:28:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working on a M2M project and need to interface to a wireless modem (verizon network) using CDC.&amp;nbsp; I have the wireless modem dev board working as a USB CDC Serial device when I connect it into my PC and I can send it AT commands and get responses.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also setup the expresso board able to be seen as a CDC Serial device using the CDC example code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But now, I need to make the LPC1769 the actual Host Controller to talk to the wireless modem.&amp;nbsp; I've been hacking on the USBHostLite example code, but it fails at HOST_GET_DESCRIPTOR() inside Host_EnumDev().&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When it fails, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TDHead-&amp;gt;Control == 0x5e040000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Bit 18 is set, which means CRC/Time Out Error according to:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://download.intel.com/technology/usb/uhci11d.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas on why the device won't enumerate?&amp;nbsp; Is USBHostLite too "Lite" to handle a CDC Serial device?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Andrew&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:09:56 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:09:56Z</dc:date>
    <item>
      <title>LPC1769 as USB Host Controller for CDC</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-as-USB-Host-Controller-for-CDC/m-p/559124#M15321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by muamw10 on Wed Feb 29 13:28:17 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working on a M2M project and need to interface to a wireless modem (verizon network) using CDC.&amp;nbsp; I have the wireless modem dev board working as a USB CDC Serial device when I connect it into my PC and I can send it AT commands and get responses.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also setup the expresso board able to be seen as a CDC Serial device using the CDC example code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But now, I need to make the LPC1769 the actual Host Controller to talk to the wireless modem.&amp;nbsp; I've been hacking on the USBHostLite example code, but it fails at HOST_GET_DESCRIPTOR() inside Host_EnumDev().&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When it fails, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TDHead-&amp;gt;Control == 0x5e040000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Bit 18 is set, which means CRC/Time Out Error according to:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://download.intel.com/technology/usb/uhci11d.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas on why the device won't enumerate?&amp;nbsp; Is USBHostLite too "Lite" to handle a CDC Serial device?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Andrew&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1769-as-USB-Host-Controller-for-CDC/m-p/559124#M15321</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:09:56Z</dc:date>
    </item>
  </channel>
</rss>