<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UDP Sample in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/UDP-Sample/m-p/529513#M1523</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Mar 22 14:45:22 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a working sample. It's transmitting a message to SOURCE_IP / SOURCE_PORT (string and number) and displaying it via semihosting.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's expecting a message from TARGET_IP / TARGET_PORT (string and number) with same format like transmitted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tested this with Windows (Win7/32) without problems (Debug and Release mode).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ARP and ICMP are working, so pinging this SOURCE_IP (or Scanner like &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.softperfect.com/products/networkscanner/&lt;/A&gt;&lt;SPAN&gt;) are working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To use it in your network you just have to use a valid SOURCE_IP/TARGET_IP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I've changed a few things in included udpip library from Aart (see notes in udpip.c).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:01:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:01:23Z</dc:date>
    <item>
      <title>UDP Sample</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UDP-Sample/m-p/529513#M1523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Mar 22 14:45:22 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a working sample. It's transmitting a message to SOURCE_IP / SOURCE_PORT (string and number) and displaying it via semihosting.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It's expecting a message from TARGET_IP / TARGET_PORT (string and number) with same format like transmitted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tested this with Windows (Win7/32) without problems (Debug and Release mode).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;ARP and ICMP are working, so pinging this SOURCE_IP (or Scanner like &lt;/SPAN&gt;&lt;A href="http://"&gt;http://www.softperfect.com/products/networkscanner/&lt;/A&gt;&lt;SPAN&gt;) are working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To use it in your network you just have to use a valid SOURCE_IP/TARGET_IP.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I've changed a few things in included udpip library from Aart (see notes in udpip.c).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UDP-Sample/m-p/529513#M1523</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:01:23Z</dc:date>
    </item>
  </channel>
</rss>