<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: Setting STACK_OFFSET automatically?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556325#M14073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Sat Feb 23 07:05:36 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I love it!&amp;nbsp;&amp;nbsp; That is great, thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pete.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:36:10 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:36:10Z</dc:date>
    <item>
      <title>Setting STACK_OFFSET automatically?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556322#M14070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Fri Feb 22 11:00:02 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Some time ago I fought a weird problem because I didn't know that&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;you had to reserve 32 bytes at the top of RAM for the IAP routines.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;With help from this group I reserved the 32 bytes and all was well.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That was a few versions of LPCXpresso ago.&amp;nbsp;&amp;nbsp; With the periodic upgrades&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I lost the setting.&amp;nbsp;&amp;nbsp; It is pretty obscure and burried down in many layers of&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;menus.&amp;nbsp;&amp;nbsp; There has to be a better way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If it is not possible for the environment to determine automatically if you &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;are using IAP then there should be some #define that you can put in your &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;code to cause the 32 bytes to be reserved.&amp;nbsp;&amp;nbsp; I suggest something like:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define&amp;nbsp;&amp;nbsp; USING_IAP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;or&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define&amp;nbsp;&amp;nbsp; IAP_RESERVED&amp;nbsp;&amp;nbsp;&amp;nbsp; 32&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If there is already something like this I would be happy to learn about it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pete.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556322#M14070</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:36:08Z</dc:date>
    </item>
    <item>
      <title>Re: Setting STACK_OFFSET automatically?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556323#M14071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Fri Feb 22 15:15:07 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The option you need to set is in the Linker settings in Project Properties. The FAQ "Reserving RAM for IAP Flash Programming"&amp;nbsp; describes exactly how to do this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/ReserveIAPRam&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using a define here wouldn't help, the value needs passing to the linker script, which doesn't use the C preprocessor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556323#M14071</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:36:08Z</dc:date>
    </item>
    <item>
      <title>Re: Setting STACK_OFFSET automatically?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556324#M14072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Sat Feb 23 04:57:53 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;It would be much better if the code just crashed when you used IAP without setting the stack offset. Since it is so easy to miss, and that the bugs produced are so subtle, this issue is a real killer.&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;Then add a reminder &lt;SPAN class="lia-unicode-emoji" title=":winking_face:"&gt;&lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
extern uint32_t _vStackTop;
extern uint32_t __top_RamLoc8;

int main(void)
{
 uint32_t offset = (uint32_t)&amp;amp;__top_RamLoc8 - (uint32_t)&amp;amp;_vStackTop;
 printf("Top of RAM(%X) - Top of Stack(%X)\n",&amp;amp;__top_RamLoc8,&amp;amp;_vStackTop);
 printf("Offset = %d\n",offset);
 if(offset &amp;lt;32)
 {
&amp;nbsp; while(1)printf("[COLOR=Red]I have forgotten to set my OFFSET[/COLOR] &amp;gt;=32!\n");
 }
 ...
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556324#M14072</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:36:09Z</dc:date>
    </item>
    <item>
      <title>Re: Setting STACK_OFFSET automatically?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556325#M14073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Sat Feb 23 07:05:36 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I love it!&amp;nbsp;&amp;nbsp; That is great, thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Pete.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Setting-STACK-OFFSET-automatically/m-p/556325#M14073</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:36:10Z</dc:date>
    </item>
  </channel>
</rss>