<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556160#M14017</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Dec 08 04:32:59 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;So FreeRTOS steel use CAN on-chip RAM. therefore nothing work. &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;No one is using illegal RAM here :eek: If it's used you failed to reserve it :rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#1 Obviously you didn't change your own linker script. I suppose you're still running with Managed linker script.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#2 Which CAN speed are you trying to receive and which main clock speed are you trying to run?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:47:05 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:47:05Z</dc:date>
    <item>
      <title>FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556143#M14000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 04:33:22 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello! I built FreeRTOS project by using example from this thred &lt;/SPAN&gt;&lt;A href="http://" rel="nofollow noopener noreferrer" target="_blank"&gt;http://knowledgebase.nxp.com/showthread.php?t=2601&lt;/A&gt;&lt;SPAN&gt;. I added to it some CAN operations (they are all from CAN)on-chip example). All FreeRtos configurations are the same. Here a code&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
...
includes
...

#define NULL&amp;nbsp;&amp;nbsp;&amp;nbsp; ((void *)0)


ROM **rom = (ROM **)0x1fff1ff8;

CAN_MSG_OBJ msg_obj;

/* Initialize CAN Controller */
uint32_t ClkInitTable[2] = {
&amp;nbsp; 0x00000005UL, // CANCLKDIV
&amp;nbsp; 0x00000103UL&amp;nbsp; // CAN_BTR
};

/* Callback function prototypes */
void CAN_rx(uint8_t msg_obj_num);
void CAN_tx(uint8_t msg_obj_num);
void CAN_error(uint32_t error_info);

/* Publish CAN Callback Functions */
CAN_CALLBACKS callbacks = {
&amp;nbsp;&amp;nbsp; CAN_rx,
&amp;nbsp;&amp;nbsp; CAN_tx,
&amp;nbsp;&amp;nbsp; CAN_error,
&amp;nbsp;&amp;nbsp; NULL,
&amp;nbsp;&amp;nbsp; NULL,
&amp;nbsp;&amp;nbsp; NULL,
&amp;nbsp;&amp;nbsp; NULL,
&amp;nbsp;&amp;nbsp; NULL,
};

/*CAN receive callback */
/*Function is executed by the Callback handler after
a CAN message has been received */
void CAN_rx(uint8_t msg_obj_num){

&amp;nbsp; /* Determine which CAN message has been received */
&amp;nbsp; msg_obj.msgobj = msg_obj_num;

&amp;nbsp; /* Now load up the msg_obj structure with the CAN message */
&amp;nbsp; (*rom)-&amp;gt;pCAND-&amp;gt;can_receive(&amp;amp;msg_obj);

&amp;nbsp; if (msg_obj_num == 1)
&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Simply transmit CAN frame (echo) with with ID +0x100 via buffer 2 */
&amp;nbsp;&amp;nbsp;&amp;nbsp; msg_obj.msgobj = 2;
&amp;nbsp;&amp;nbsp;&amp;nbsp; msg_obj.mode_id += 0x100;
&amp;nbsp;&amp;nbsp;&amp;nbsp; (*rom)-&amp;gt;pCAND-&amp;gt;can_transmit(&amp;amp;msg_obj);
&amp;nbsp; }

&amp;nbsp; return;
}

/*CAN transmit callback */
/*Function is executed by the Callback handler after
a CAN message has been transmitted */
void CAN_tx(uint8_t msg_obj_num){
&amp;nbsp; return;
}

/*CAN error callback */
/*Function is executed by the Callback handler after
an error has occured on the CAN bus */
void CAN_error(uint32_t error_info){
&amp;nbsp; return;
}

/*CAN interrupt handler */
/*The CAN interrupt handler must be provided by the user application.
It's function is to call the isr() API located in the ROM */
void CAN_IRQHandler (void){
&amp;nbsp; (*rom)-&amp;gt;pCAND-&amp;gt;isr();
}

// TASKS================================================================================================
void vApplicationStackOverflowHook( xTaskHandle *pxTask, signed portCHAR *pcTaskName )
{
;
}

void vApplicationIdleHook( void )
{
__WFI();
}

void vTaskCANint(void *pvParameters)
{
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* vTaskCANint executed */
LPC_GPIO2-&amp;gt;DATA |= 2;
msg_obj.msgobj&amp;nbsp; = 0;
msg_obj.mode_id = 0x345;
msg_obj.mask&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x0;
msg_obj.dlc&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4;
msg_obj.data[0] = 'T';//0x54
msg_obj.data[1] = 'E';//0x45
msg_obj.data[2] = 'S';//0x53
msg_obj.data[3] = 'T';//0x54
(*rom)-&amp;gt;pCAND-&amp;gt;can_transmit(&amp;amp;msg_obj);
while(1)
{
;
}
}

void vTaskempty(void *pvParameters)
{
LPC_GPIO2-&amp;gt;DATA |= 1;
/* vTaskempty executed */
msg_obj.msgobj&amp;nbsp; = 0;
msg_obj.mode_id = 0x345;
msg_obj.mask&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x0;
msg_obj.dlc&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4;
msg_obj.data[0] = 'T';//0x54
msg_obj.data[1] = 'E';//0x45
msg_obj.data[2] = 'S';//0x53
msg_obj.data[3] = 'T';//0x54
(*rom)-&amp;gt;pCAND-&amp;gt;can_transmit(&amp;amp;msg_obj);
while(1)
{
;
}
}
//======================================================================================================

int main(void) {

/* Output the Clk onto the CLKOUT Pin PIO0_1 to monitor the freq on a scope */
LPC_IOCON-&amp;gt;PIO0_1= (1&amp;lt;&amp;lt;0);
/* Select the MAIN clock as the clock out selection since it's driving the core */
LPC_SYSCON-&amp;gt;CLKOUTCLKSEL = 3;
/* Set CLKOUTDIV to 6 */
LPC_SYSCON-&amp;gt;CLKOUTDIV = 10;//CLKOUT Divider = 10
/* Enable CLKOUT */
LPC_SYSCON-&amp;gt;CLKOUTUEN = 0;
LPC_SYSCON-&amp;gt;CLKOUTUEN = 1;
while (!(LPC_SYSCON-&amp;gt;CLKOUTUEN &amp;amp; 0x01));

/* Initialize the CAN controller */
(*rom)-&amp;gt;pCAND-&amp;gt;init_can(&amp;amp;ClkInitTable[0], 1);

/* Configure the CAN callback functions */
(*rom)-&amp;gt;pCAND-&amp;gt;config_calb(&amp;amp;callbacks);

/* Enable the CAN Interrupt */
NVIC_EnableIRQ(CAN_IRQn);

/* Send a simple one time CAN message */
msg_obj.msgobj&amp;nbsp; = 0;
msg_obj.mode_id = 0x345;
msg_obj.mask&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x0;
msg_obj.dlc&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4;
msg_obj.data[0] = 'T';//0x54
msg_obj.data[1] = 'E';//0x45
msg_obj.data[2] = 'S';//0x53
msg_obj.data[3] = 'T';//0x54
(*rom)-&amp;gt;pCAND-&amp;gt;can_transmit(&amp;amp;msg_obj);

/* Configure message object 1 to receive all 11-bit messages 0x400-0x4FF */
msg_obj.msgobj = 1;
msg_obj.mode_id = 0x400;
msg_obj.mask = 0x700;
(*rom)-&amp;gt;pCAND-&amp;gt;config_rxmsgobj(&amp;amp;msg_obj);

//creating tasks----------------------------------------------------------
xTaskCreate( vTaskCANint, (const signed portCHAR * const)"ping", configMINIMAL_STACK_SIZE,
NULL, 3, NULL);
xTaskCreate( vTaskempty, (const signed portCHAR * const)"counter", configMINIMAL_STACK_SIZE,
NULL, 3, NULL);
//------------------------------------------------------------------------

 LPC_GPIO2-&amp;gt;DIR |= 0x3;
&amp;nbsp; LPC_GPIO2-&amp;gt;DATA = 0;

vTaskStartScheduler();

/* if starting Scheduler is failed&amp;nbsp; */
msg_obj.msgobj&amp;nbsp; = 0;
msg_obj.mode_id = 0x000;
msg_obj.mask&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x0;
msg_obj.dlc&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 4;
msg_obj.data[0] = 0xFF;//0x54
msg_obj.data[1] = 0xFF;//0x45
msg_obj.data[2] = 0xFF;//0x53
msg_obj.data[3] = 0xFF;//0x54
(*rom)-&amp;gt;pCAND-&amp;gt;can_transmit(&amp;amp;msg_obj);

while(1){
__WFI();/* Go to Sleep */
}
}

&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;SPAN&gt;So program stops executing (interrupts don't work too) at vTaskStartScheduler();. actually program stops at vPortStartFirstTask() in xPortStartScheduler(). What is wrong? Please help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;void SVCall_Handler(void) execute when vPortStartFirstTask() try to start. In SVCall_Handler while(1) so program is cycled.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556143#M14000</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:54Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556144#M14001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Dec 07 05:35:23 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;What is wrong?&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;OK, you've asked :rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#1 You don't post your project, so someone who's trying to help has to ask about settings again and again....&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#2 You are using CAN on-chip code parts to copy them into other projects. What did you do to protect On-chip RAM?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See user manual:&lt;/SPAN&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;14.4.1 Calling the C_CAN API&lt;BR /&gt;... On-chip RAM from address 0x1000 0050 to 0x1000 00B8 is used by the CAN API. This address&lt;BR /&gt;range should not be used by the application. For applications using the on-chip CAN API,&lt;BR /&gt;the linker control file should be modified appropriately to prevent usage of this area for&lt;BR /&gt;application’s variable storage...&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556144#M14001</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556145#M14002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 05:41:00 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;OK, you've asked :rolleyes:&lt;BR /&gt;&lt;BR /&gt;#1 You don't post your project, so someone who's trying to help has to ask about settings again and again....&lt;BR /&gt;&lt;BR /&gt;#2 You are using CAN on-chip code parts to copy them into other projects. What did you do to protect On-chip RAM?&lt;BR /&gt;&lt;BR /&gt;See user manual:&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;amp;#1054;&amp;amp;#1082;. Here is my project.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556145#M14002</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:56Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556146#M14003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 05:42:04 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;OK, you've asked :rolleyes:&lt;BR /&gt;&lt;BR /&gt;#2 You are using CAN on-chip code parts to copy them into other projects. What did you do to protect On-chip RAM?&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Haw should I protect On-chip RAM?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556146#M14003</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556147#M14004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by stalisman on Wed Dec 07 07:37:28 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Howdy,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You seem to have a problem with the [B]cr_startup_lpc11.c[/B] file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It doesn't for example include the functions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][LEFT]WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]vPortSVCHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]xPortPendSVHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]xPortSysTickHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);[/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2]that are defined in port.c.[/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2]If you use these in the table instead:[/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][LEFT]vPortSVCHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// SVCall handler[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]0, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// Reserved[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]0, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// Reserved[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]xPortPendSVHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// The PendSV handler[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]xPortSysTickHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// The SysTick handler[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// [U]Wakeup[/U] sources for the I/O pins:[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT][/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// PIO0 (0:11)[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// PIO1 (0)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2]then FreeRTOS runs your tasks.[/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE] &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2](note I ran it up on a LPC1114 after knocking out the CAN stuff so I don't know if those bits are ok).[/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556147#M14004</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556148#M14005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 09:11:15 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: stalisman&lt;/STRONG&gt;&lt;BR /&gt;Howdy,&lt;BR /&gt; &lt;BR /&gt;You seem to have a problem with the [B]cr_startup_lpc11.c[/B] file.&lt;BR /&gt; &lt;BR /&gt;It doesn't for example include the functions:&lt;BR /&gt; &lt;BR /&gt;[SIZE=2][LEFT]WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]vPortSVCHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);&lt;BR /&gt;WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]xPortPendSVHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);[/LEFT]&lt;BR /&gt;WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]xPortSysTickHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2]that are defined in port.c.[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2]If you use these in the table instead:[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2][LEFT]vPortSVCHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// SVCall handler[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]0, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// Reserved[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]0, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// Reserved[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]xPortPendSVHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// The PendSV handler[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]xPortSysTickHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// The SysTick handler[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]&lt;BR /&gt;[/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// [U]Wakeup[/U] sources for the I/O pins:[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT][/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// PIO0 (0:11)[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// PIO1 (0)&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2]then FreeRTOS runs your tasks.[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2](note I ran it up on a LPC1114 after knocking out the CAN stuff so I don't know if those bits are ok).[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE]&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, I do not quite understand. Should I change vPortSVCHandler on something else?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556148#M14005</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556149#M14006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by stalisman on Wed Dec 07 09:18:42 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have attached an edited version of the file ... just do a windiff and see :-)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556149#M14006</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556150#M14007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 09:25:17 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: stalisman&lt;/STRONG&gt;&lt;BR /&gt;Howdy,&lt;BR /&gt; &lt;BR /&gt;You seem to have a problem with the [B]cr_startup_lpc11.c[/B] file.&lt;BR /&gt; &lt;BR /&gt;It doesn't for example include the functions:&lt;BR /&gt; &lt;BR /&gt;[SIZE=2][LEFT]WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]vPortSVCHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);&lt;BR /&gt;WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]xPortPendSVHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);[/LEFT]&lt;BR /&gt;WEAK [/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2] [B]xPortSysTickHandler[/B]([/SIZE][B][SIZE=2][COLOR=#7f0055][SIZE=2][COLOR=#7f0055]void[/B][/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2]);[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2]that are defined in port.c.[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2]If you use these in the table instead:[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2][LEFT]vPortSVCHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// SVCall handler[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]0, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// Reserved[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]0, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// Reserved[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]xPortPendSVHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// The PendSV handler[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]xPortSysTickHandler, [/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// The SysTick handler[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT]&lt;BR /&gt;[/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// [U]Wakeup[/U] sources for the I/O pins:[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][LEFT][/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// PIO0 (0:11)[/LEFT]&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][/SIZE][SIZE=2][COLOR=#3f7f5f][SIZE=2][COLOR=#3f7f5f]// PIO1 (0)&lt;BR /&gt;[/COLOR][/SIZE][/COLOR][/SIZE][SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2]then FreeRTOS runs your tasks.[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE] &lt;BR /&gt;[SIZE=2](note I ran it up on a LPC1114 after knocking out the CAN stuff so I don't know if those bits are ok).[/SIZE]&lt;BR /&gt;[SIZE=2][/SIZE]&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: stalisman&lt;/STRONG&gt;&lt;BR /&gt;Hi,&lt;BR /&gt; &lt;BR /&gt;I have attached an edited version of the file ... just do a windiff and see :-)&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So is there&amp;nbsp; need just to comment this lines?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; /*&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WEAK void SVCall_Handler(void);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WEAK void PendSV_Handler(void);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WEAK void SysTick_Handler(void);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;*/&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Unfortunately, I don't have LPCXpresso at the moment, but I'll check tomorrow. Thank, very match!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556150#M14007</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556151#M14008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 21:23:33 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;It didn't help ((. Haw to protect CAN_on-chip RAM?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556151#M14008</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556152#M14009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Dec 07 21:27:41 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Reserve it :eek:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you meanwhile check your map file if someone is using CAN on-chip RAM ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556152#M14009</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556153#M14010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 21:38:35 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;Reserve it :eek:&lt;BR /&gt;&lt;BR /&gt;Did you meanwhile check your map file if someone is using CAN on-chip RAM ?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Well, it seems there is really something&amp;nbsp; use CAN on-chip RAM... And the the most stupid question in this thread: Haw to reserve it?:o&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556153#M14010</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556154#M14011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Dec 07 22:27:21 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There are several options. You could use cr_section_macros.h without own linker script or you can just change your own linker script to fill 0xC0 bytes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : AT (__exidx_end)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {
[COLOR=Red]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FILL(0x00);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; . = 0x000000C0;[/COLOR]
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _data = .;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *(vtable)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *(.data*)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _edata = .;
&amp;nbsp;&amp;nbsp;&amp;nbsp; } &amp;gt; RamLoc8
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556154#M14011</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556155#M14012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Wed Dec 07 23:54:12 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;There are several options. You could use cr_section_macros.h without own linker script or you can just change your own linker script to fill 0xC0 bytes:&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : AT (__exidx_end)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {
[COLOR=Red]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FILL(0x00);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; . = 0x000000C0;[/COLOR]
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _data = .;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *(vtable)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *(.data*)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _edata = .;
&amp;nbsp;&amp;nbsp;&amp;nbsp; } &amp;gt; RamLoc8
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My linker don't have those lines (CAN_on-chip_Debug_lib.ld). I added your code to the linker fully. After that I tried change CAN_on-chip_Debug_lib_mem.ld to this (I read about it in &lt;/SPAN&gt;&lt;A href="http://http://www.nxp.com/documents/application_note/AN10905.pdf" rel="nofollow noopener noreferrer" target="_blank"&gt;appnout for lpc13xx&lt;/A&gt;&lt;SPAN&gt; page 5):&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;

MEMORY
{
&amp;nbsp; /* Define each memory region */
&amp;nbsp; MFlash32 (rx) : ORIGIN = 0x0, LENGTH = 0x8000 /* 32k */
[COLOR=Red]&amp;nbsp; RamLoc8 (rwx) : ORIGIN = 0x100000B8, LENGTH = 0x1F48 /* 8k */[/COLOR]

}
&amp;nbsp; /* Define a symbol for the top of each memory region */
&amp;nbsp; __top_MFlash32 = 0x0 + 0x8000;
[COLOR=Red]&amp;nbsp;&amp;nbsp; __top_RamLoc8 = 0x100000B8 + 0x1F48; [/COLOR]

&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It didn't help too. Haw to use cr_section_macros.h to protect&amp;nbsp; CAN on-chip ram?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556155#M14012</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:02Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556156#M14013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Dec 08 00:26:57 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;It didn't help too.&amp;nbsp; :confused:&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;To do what? To fill RAM from 0x10000000 to 0x1000000BF?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556156#M14013</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556157#M14014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by yanvasilij on Thu Dec 08 00:48:00 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;To do what? To fill RAM from 0x10000000 to 0x1000000BF?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;here is part of map file:&lt;/SPAN&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
 .data.SystemCoreClock
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000034&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x4 ./src/system_LPC11xx.o
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000034&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClock
 .data.xNextTaskUnblockTime
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000038&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x4 ./src/tasks.o
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1000003c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; . = ALIGN (0x4)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1000003c&amp;nbsp; 
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So FreeRTOS steel use CAN on-chip RAM. therefore nothing work.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556157#M14014</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556158#M14015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Rob65 on Thu Dec 08 01:25:01 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This just means that you did not reserve a section in memory for the RAM that is used by the on chip CAN driver. So your attempt to reserve memory in the .ld file failed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please check again if you made the proper changes and if you changed the file being used (this would not be the first time someone changed a file that is not being used at all...).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you exactly followed the instruction in the App Note you referred to then you should have created a set of new linker files that are being used. Please only follow this procedure - do not change the default files by hand (they may be overwritten) and make sure that you are using the new files by e.g. making a typo in the file and try to link again - this should result in an error meaning that you are changing the correct file :cool:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Rob&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556158#M14015</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:04Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556159#M14016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by stalisman on Thu Dec 08 03:26:56 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am a little curiousc...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it significant or not that Section 14.4.2 of UM10398 has the following code? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[LEFT][FONT=Arial][SIZE=2][FONT=Arial][SIZE=2]Example call:[/SIZE][/FONT][/SIZE][/FONT][FONT=Arial][SIZE=2]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT][FONT=Courier][SIZE=2][FONT=Courier][SIZE=2]ROM **rom = (ROM **)(0x1fff1ff8[B] + 2 * sizeof(ROM **));[/B][/SIZE][/FONT][/SIZE][/FONT][FONT=Courier][SIZE=2]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][FONT=Courier]uint32_t CanApiClkInitTable[2] = {[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][FONT=Courier]0x00000000UL, // CANCLKDIV[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][FONT=Courier]0x00004DC5UL // CAN_BTR[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][FONT=Courier]};[/FONT][/SIZE][/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][FONT=Courier](*rom)-&amp;gt;pCANAPI-&amp;gt;init_can(&amp;amp;CanApiCanInitTable[0]);[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][FONT=Courier]it differs slightly from that presented earlier.[/FONT][/SIZE]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE][/FONT]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556159#M14016</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:04Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556160#M14017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Dec 08 04:32:59 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;So FreeRTOS steel use CAN on-chip RAM. therefore nothing work. &lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;No one is using illegal RAM here :eek: If it's used you failed to reserve it :rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#1 Obviously you didn't change your own linker script. I suppose you're still running with Managed linker script.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#2 Which CAN speed are you trying to receive and which main clock speed are you trying to run?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556160#M14017</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:05Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556161#M14018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by stalisman on Thu Dec 08 05:30:02 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Zero&lt;/STRONG&gt;&lt;BR /&gt;No one is using illegal RAM here :eek: If it's used you failed to reserve it :rolleyes:&lt;BR /&gt; &lt;BR /&gt;#1 Obviously you didn't change your own linker script. I suppose you're still running with Managed linker script.&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi guys,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;re #1: FreeRtos is placing its heap in the CAN area.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I followed the 'Modifying Linker Scripts' tutorial at &lt;/SPAN&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/training/lpcxpresso.intro.2/&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.. and managed to reserve the space. The tutorial reserves a tad too much but the ideas are sound.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556161#M14018</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:06Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS + LPC11C14 + CAN_on-chip</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556162#M14019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu Dec 08 06:07:12 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I like this historical videos from NXP Discovery Channel :rolleyes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course the modern version is more elegant. Since V3.6 :eek: it's easier to use Managed linker scripts and section macros of cr_section_macros.h.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then adding 1 :)&amp;nbsp; line of code is enough:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;__BSS(RESERVED) char CAN_driver_memory[0xC0];&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See 'Reserved Memory Regions' in &lt;/SPAN&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/EnhancedManagedLinkScripts&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And best of all: Project Wizard is including all this section stuff in my new project if I'm not too dumb to select 'Enable CRP in target image' :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/FreeRTOS-LPC11C14-CAN-on-chip/m-p/556162#M14019</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:47:06Z</dc:date>
    </item>
  </channel>
</rss>