<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックprogramming to flash</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/programming-to-flash/m-p/555553#M13745</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gudushen on Fri Aug 05 09:24:01 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two binary files I need to program into a LPC1754, using lpcxpresso&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;one at flash address 0x00 and one at 0x1E000 but I don't know how?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried using the program flash option in binary utilities, but I can't set the base address other than 0x00?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any help is appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:13:33 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:13:33Z</dc:date>
    <item>
      <title>programming to flash</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/programming-to-flash/m-p/555553#M13745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gudushen on Fri Aug 05 09:24:01 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two binary files I need to program into a LPC1754, using lpcxpresso&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;one at flash address 0x00 and one at 0x1E000 but I don't know how?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried using the program flash option in binary utilities, but I can't set the base address other than 0x00?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any help is appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:13:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/programming-to-flash/m-p/555553#M13745</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:13:33Z</dc:date>
    </item>
  </channel>
</rss>