<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debug configuration set to point at GDB (build with python included).  in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555279#M13613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, there does seem to be an issue here. We'll look at fixing this in a future product release, but in the meantime, you can achieve your requirement in one of the following two ways...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case that you have a project which does not yet have a launch configuration file (or where you are happy to delete the existing launch configuration file), then the simplest way to solve this is to go to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Preferences - LPCXpresso - Debug Options (Miscellaneous)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and change the Debugger Executable from "&lt;STRONG&gt;arm-none-eabi-gdb&lt;/STRONG&gt;" to "&lt;STRONG&gt;arm-none-eabi-gdb-py&lt;/STRONG&gt;". This setting will then get picked up when you first debug your project (when the IDE will automatically create a new launch configuration file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or to update an existing launch configuration, double click on the .launch file inside your project (in the Project Explorer view) to open it in the editor. Then change the line:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;lt;stringAttribute key="org.eclipse.cdt.dsf.gdb.DEBUG_NAME" value="arm-none-eabi-gdb"/&amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;lt;stringAttribute key="org.eclipse.cdt.dsf.gdb.DEBUG_NAME" value="arm-none-eabi-gdb-py"/&amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jul 2016 10:46:46 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-07-11T10:46:46Z</dc:date>
    <item>
      <title>Debug configuration set to point at GDB (build with python included).</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555278#M13612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Continues to use LPCxpresso version of GDB. Set in "Debug Configuration" "Debugger" "Main" to point to another version of GDB.&amp;nbsp; Looks like it is ignoring the selection and always using the LPCxpresso version of GDB. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 18:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555278#M13612</guid>
      <dc:creator>thomascurry</dc:creator>
      <dc:date>2016-07-09T18:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: Debug configuration set to point at GDB (build with python included).</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555279#M13613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, there does seem to be an issue here. We'll look at fixing this in a future product release, but in the meantime, you can achieve your requirement in one of the following two ways...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case that you have a project which does not yet have a launch configuration file (or where you are happy to delete the existing launch configuration file), then the simplest way to solve this is to go to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Preferences - LPCXpresso - Debug Options (Miscellaneous)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and change the Debugger Executable from "&lt;STRONG&gt;arm-none-eabi-gdb&lt;/STRONG&gt;" to "&lt;STRONG&gt;arm-none-eabi-gdb-py&lt;/STRONG&gt;". This setting will then get picked up when you first debug your project (when the IDE will automatically create a new launch configuration file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or to update an existing launch configuration, double click on the .launch file inside your project (in the Project Explorer view) to open it in the editor. Then change the line:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;lt;stringAttribute key="org.eclipse.cdt.dsf.gdb.DEBUG_NAME" value="arm-none-eabi-gdb"/&amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;lt;stringAttribute key="org.eclipse.cdt.dsf.gdb.DEBUG_NAME" value="arm-none-eabi-gdb-py"/&amp;gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2016 10:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555279#M13613</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-07-11T10:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: Debug configuration set to point at GDB (build with python included).</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555280#M13614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good solution.&amp;nbsp; Works better than my way to allow all future debug configurations to use selected GDB application.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2016 14:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Debug-configuration-set-to-point-at-GDB-build-with-python/m-p/555280#M13614</guid>
      <dc:creator>thomascurry</dc:creator>
      <dc:date>2016-07-11T14:21:26Z</dc:date>
    </item>
  </channel>
</rss>