<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC11E11 debugging problem with LPCxpresso 6 in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554848#M13405</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Donatas on Sun Dec 29 03:41:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the answer. The reason was not the flash driver, as you said. The problem was incorrect include in one of the project files. I have included "lpc11xx.h" instead of "lpc11exx.h".&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:03:19 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:03:19Z</dc:date>
    <item>
      <title>LPC11E11 debugging problem with LPCxpresso 6</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554846#M13403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Donatas on Sat Dec 28 04:43:47 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyone tried debugging LPC11E11 device using LPCxresso? I have some problems related to Flash driver. By default LPC11_12_13_8K_4K.cfx should be used, but it does not exist in lpcxpresso_6.1.2_177/lpcxpresso/bin/Flash folder. If I use LPC11_12_13_8K_2K.cfx file, debugging always ends in void HardFault_Handler(void) subroutine. Not sure if it happens because of incorrect initialization of MCU clocks, etc, or because of flash driver. Did you have any problems like this before?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554846#M13403</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11E11 debugging problem with LPCxpresso 6</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554847#M13404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Sat Dec 28 16:08:40 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry for not supplying that flash driver (we will fix that in the next release). However, the alternate you suggest does work correctly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are getting a hard fault, this is most likely a problem in your code. I suggest you start debugging from ResetISR and step through the code to find the cause of the fault.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554847#M13404</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11E11 debugging problem with LPCxpresso 6</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554848#M13405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Donatas on Sun Dec 29 03:41:26 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the answer. The reason was not the flash driver, as you said. The problem was incorrect include in one of the project files. I have included "lpc11xx.h" instead of "lpc11exx.h".&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11E11-debugging-problem-with-LPCxpresso-6/m-p/554848#M13405</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:03:19Z</dc:date>
    </item>
  </channel>
</rss>