<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC1100 FFT Function</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1100-FFT-Function/m-p/554736#M13359</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanMorris on Thu Jun 24 15:25:01 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The attached zip file contains an implementation of a 256-point FFT function for the Cortex-M0 family of products (LPC1100 devices) along with example projects for the Keil, IAR and CodeRed Software Development platforms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The original implementation was kindly supplied by Chris Guarneri of NXP. The FFT function is provided as a prebuilt library file. The source for the FFT function is not supplied as it is based upon code that is only available from NXP under NDA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hopefully this will be of use to someone....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:12:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:12:39Z</dc:date>
    <item>
      <title>LPC1100 FFT Function</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1100-FFT-Function/m-p/554736#M13359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by IanMorris on Thu Jun 24 15:25:01 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The attached zip file contains an implementation of a 256-point FFT function for the Cortex-M0 family of products (LPC1100 devices) along with example projects for the Keil, IAR and CodeRed Software Development platforms.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The original implementation was kindly supplied by Chris Guarneri of NXP. The FFT function is provided as a prebuilt library file. The source for the FFT function is not supplied as it is based upon code that is only available from NXP under NDA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hopefully this will be of use to someone....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:12:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1100-FFT-Function/m-p/554736#M13359</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:12:39Z</dc:date>
    </item>
  </channel>
</rss>