<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1114 without external crystal in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554734#M13357</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Mon Mar 07 14:27:24 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;A few lines above you find:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_SYSCON-&amp;gt;SYSPLLCLKSEL = SYSPLLCLKSEL_Val; /* Select PLL Input &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This value sets the PLL circuit input source (see table 15 UM10398).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If it's 1 you try to use 'system oscillator' = crystal. Could be a problem :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you change it to 0, you can use IRC = internal RC oscillator (12MHz)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: IRC accuracy is just 1%&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:05:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:05:23Z</dc:date>
    <item>
      <title>LPC1114 without external crystal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554732#M13355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by chucks13 on Mon Mar 07 11:46:33 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, I am new to the forums, so if the is an FAQ, please forgive me&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a target board based on the LPCXpresso 1114 board. My target board has no crystal, because I was assured that it run without it using the PLL to drive the system clock, up to at least 48 Mhz, and hopefully 50. The standard examples which I believe are suppose to activate the PLL have on this line:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; while (!(LPC_SYSCON-&amp;gt;SYSPLLSTAT &amp;amp; 0x01));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait Until PLL Locked&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is in the library SystemInit() function. My board makes it to this line and hangs. The obvious reason is that the PLL never acquires a lock. I have not made any changes to the initialization code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I fear that I have missed something, like an external resistor that the LPCXpresso&amp;nbsp; board with the crystal doesn't need, or the standard examples&amp;nbsp; needs something more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for reading my post.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Chuck&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554732#M13355</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114 without external crystal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554733#M13356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Luis Digital on Mon Mar 07 11:59:03 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;View: &lt;/SPAN&gt;&lt;A href="http://http://knowledgebase.nxp.com/showthread.php?t=228&amp;amp;highlight=LPC1111"&gt;[B]LPC11xx basics required[/B]&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554733#M13356</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114 without external crystal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554734#M13357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Mon Mar 07 14:27:24 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;A few lines above you find:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_SYSCON-&amp;gt;SYSPLLCLKSEL = SYSPLLCLKSEL_Val; /* Select PLL Input &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This value sets the PLL circuit input source (see table 15 UM10398).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If it's 1 you try to use 'system oscillator' = crystal. Could be a problem :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you change it to 0, you can use IRC = internal RC oscillator (12MHz)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: IRC accuracy is just 1%&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554734#M13357</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114 without external crystal</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554735#M13358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by chucks13 on Mon Mar 07 16:26:05 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;//#define SYSPLLCLKSEL_Val&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000001 // This sets to use external crystal for clock source for PLL&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define SYSPLLCLKSEL_Val&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000000 // Set PLL input to internal RC oscillator&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you. This fixed my problem.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:05:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1114-without-external-crystal/m-p/554735#M13358</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:05:24Z</dc:date>
    </item>
  </channel>
</rss>