<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic User App does not work... in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/User-App-does-not-work/m-p/554654#M13338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alanisgp on Wed Mar 07 06:04:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, I have successfully managed to run the application, in fact, download the binary image and burn it to flash. The problem I have found then is that it hangs when trying to run the user application. I followed all the steps to create the corresponding script link to the binary image.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Why not run?. The question that arises if the initialized data from the user application are copied from flash to RAM, as this is done by ResetISR (), which, from the point of view of the execution of the secondary bootloader is never invoked in the user application as a reset is not effected due to routing is performed by a jump of code.??? Any suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Thank you very much and best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:04:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:04:47Z</dc:date>
    <item>
      <title>User App does not work...</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/User-App-does-not-work/m-p/554654#M13338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alanisgp on Wed Mar 07 06:04:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, I have successfully managed to run the application, in fact, download the binary image and burn it to flash. The problem I have found then is that it hangs when trying to run the user application. I followed all the steps to create the corresponding script link to the binary image.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Why not run?. The question that arises if the initialized data from the user application are copied from flash to RAM, as this is done by ResetISR (), which, from the point of view of the execution of the secondary bootloader is never invoked in the user application as a reset is not effected due to routing is performed by a jump of code.??? Any suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; Thank you very much and best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/User-App-does-not-work/m-p/554654#M13338</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:04:47Z</dc:date>
    </item>
  </channel>
</rss>