<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Lpc11c14 - header files in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpc11c14-header-files/m-p/554204#M13133</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdebliek on Mon Jun 28 12:44:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am just finishing a project with the LPC11C14.&amp;nbsp; The NXP rep had sent me the sample code the Keil and IAR generated for the part.&amp;nbsp; Attached is the header file I used.&amp;nbsp; I think I had to add the interrupt definitions to the initial file I received.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The Keil code I received does not use the CAN ROM functions, but the IAR code does.&amp;nbsp; If you plan on using the ROM functions, I would recommend getting the IAR code, as the user manual is somewhat deficient.&amp;nbsp; I did not receive this code until after a spend several days figuring it out myself.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:11:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:11:01Z</dc:date>
    <item>
      <title>Lpc11c14 - header files</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpc11c14-header-files/m-p/554203#M13132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kenako on Mon Jun 28 07:21:11 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;For the LPC11C14, do you know if LPCXpresso supports the device yet? I know it supports the &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC11xx range, however I checked the library files in the software and the LPC11C14 Header files are not implemented&amp;nbsp; yet ? The only &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;additions would be the pointers associated with the CAM block.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Lpc11c14-header-files/m-p/554203#M13132</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc11c14 - header files</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpc11c14-header-files/m-p/554204#M13133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdebliek on Mon Jun 28 12:44:14 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am just finishing a project with the LPC11C14.&amp;nbsp; The NXP rep had sent me the sample code the Keil and IAR generated for the part.&amp;nbsp; Attached is the header file I used.&amp;nbsp; I think I had to add the interrupt definitions to the initial file I received.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The Keil code I received does not use the CAN ROM functions, but the IAR code does.&amp;nbsp; If you plan on using the ROM functions, I would recommend getting the IAR code, as the user manual is somewhat deficient.&amp;nbsp; I did not receive this code until after a spend several days figuring it out myself.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Lpc11c14-header-files/m-p/554204#M13133</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:11:01Z</dc:date>
    </item>
  </channel>
</rss>