<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ssp spi cmsis1.3 examples in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/ssp-spi-cmsis1-3-examples/m-p/554119#M13084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dragilla on Wed Dec 07 10:55:18 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm probably missing something here, but help me undestand please.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the cmsis v1.3 there are some nice examples, including spi and ssp.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I undestand correcyly SSP is synchronous serial port which can operate using SPI (serial peripheral interface) or other: TI SSI, Microwire...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The question is: why some examples, like sc16is750_int, sc16is750_polling, Master, Slave are in both directories if they both use SPI and why those examples are different? :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:44:02 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:44:02Z</dc:date>
    <item>
      <title>ssp spi cmsis1.3 examples</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/ssp-spi-cmsis1-3-examples/m-p/554119#M13084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by dragilla on Wed Dec 07 10:55:18 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm probably missing something here, but help me undestand please.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the cmsis v1.3 there are some nice examples, including spi and ssp.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I undestand correcyly SSP is synchronous serial port which can operate using SPI (serial peripheral interface) or other: TI SSI, Microwire...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The question is: why some examples, like sc16is750_int, sc16is750_polling, Master, Slave are in both directories if they both use SPI and why those examples are different? :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/ssp-spi-cmsis1-3-examples/m-p/554119#M13084</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:44:02Z</dc:date>
    </item>
  </channel>
</rss>