<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックSPI Problem</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Problem/m-p/552301#M12239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersonf on Wed May 11 11:35:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am programming for the ARM LPC1343 SPI communication and am having problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I used the example of NPX for SPI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;By placing the oscilloscope on pin 2.11 (SCLK) voltage is only 350mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is a "clock"very bad .. are sequences of peaks and then stays low ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;happens again this sequence, up to half of these peaks seems that the distance of one and one equals ... but then stays the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried putting greater 4,8,10 prescaler to reduce the frequency and check if "noise" would diminish .. but to no avail.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Could someone help me solve this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:07:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:07:26Z</dc:date>
    <item>
      <title>SPI Problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Problem/m-p/552301#M12239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersonf on Wed May 11 11:35:47 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am programming for the ARM LPC1343 SPI communication and am having problems.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I used the example of NPX for SPI.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;By placing the oscilloscope on pin 2.11 (SCLK) voltage is only 350mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;There is a "clock"very bad .. are sequences of peaks and then stays low ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;happens again this sequence, up to half of these peaks seems that the distance of one and one equals ... but then stays the same.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I tried putting greater 4,8,10 prescaler to reduce the frequency and check if "noise" would diminish .. but to no avail.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Could someone help me solve this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Problem/m-p/552301#M12239</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Problem/m-p/552302#M12240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Thu May 12 06:15:18 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Which sample are we talking about?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My lpcxpresso_3.6/Examples/NXP/LPC1000/LPC13xx/examples.lpc13xx.new.zip-&amp;gt;ssp sample&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;is producing a nice clock signal at P2.11 if I add a simple write loop in main of ssptest.c:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
int main (void)
{
&amp;nbsp; uint32_t i;
&amp;nbsp; SSPInit();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // initialize SSP port, share pins with SPI0
&amp;nbsp; for ( i = 0; i &amp;lt; SSP_BUFSIZE; i++ )
&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp; src_addr&lt;I&gt; = (uint8_t)i;
&amp;nbsp;&amp;nbsp;&amp;nbsp; dest_addr&lt;I&gt; = 0;
&amp;nbsp; }
&amp;nbsp; while(1)
&amp;nbsp; {
&amp;nbsp;&amp;nbsp; SSPSend( (uint8_t *)src_addr, SSP_BUFSIZE);
&amp;nbsp; }
&amp;nbsp; return 0;
}
&lt;/I&gt;&lt;/I&gt;&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;SPAN&gt;Frequency: 2.25 MHz (as expected)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can change it without problems with:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_SYSCON-&amp;gt;SSPCLKDIV = 0x01;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Divided by 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_SSP-&amp;gt;CR0 = 0x0007;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //SCR 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;to 36 MHz (=max speed @ 72MHz clock).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/SPI-Problem/m-p/552302#M12240</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:07:27Z</dc:date>
    </item>
  </channel>
</rss>