<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: How Can I Use 2xLPCLink-2 to Develop/Debug USB Device Firmware on an LPCLink-2 board.</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551889#M12058</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sun Mar 08 04:43:50 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Do you think I would not have researched and read everything before I have to ask questions.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You didn't say what you had research and I can't read your brain from here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The issue with LPC-Link2 (LPC43xx, strictly) is only that the dfu utility can't boot if two dfu-bootable devices with the same vid/pid are connected at the same time. The exact rules for whether a device will attempt to boot is described in the manual, but basically you can stop it by configuring boot pins. Do that, and there is no issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why not go and try it?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:28:03 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:28:03Z</dc:date>
    <item>
      <title>How Can I Use 2xLPCLink-2 to Develop/Debug USB Device Firmware on an LPCLink-2 board.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551885#M12054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sat Mar 07 17:34:28 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;OK. I have read the many postings about only connecting one LPCLink-2 at a time to the PC [Win7-64].&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;But what if i have to do this?&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can the IDE team specify (at idiot level ) What to connect, in what order, with setting for all &lt;/SPAN&gt;&lt;I&gt;four&lt;/I&gt;&lt;SPAN&gt; jumpers&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(JP1, JP2 on two boards), when to connect USB cables (note plural!), when to start the application USB code&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;on the PC in order to ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Download (to target RAM) the latest edit/compile cycle and start debugging it via the probe LPCLink-2 board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NOTE WELL that I only have one PC -- multi-machine solutions need not apply!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551885#M12054</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Use 2xLPCLink-2 to Develop/Debug USB Device Firmware on an LPCLink-2 board.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551886#M12055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sat Mar 07 18:03:14 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I am &lt;/SPAN&gt;&lt;I&gt;trying&lt;/I&gt;&lt;SPAN&gt; to think for myself, would the following work?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Starting with nothing plugged in and nothing running.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[1] Plug in probe LPCLink-2 with JP1 off, JP2 off, ribbon from J7 to target J2. Target not connected/powered at this point. (Target JP1 off JP2 off also).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[2] Use DFU-Util to load Redlink on to probe. IDE still not running. [Expected that DFU capable device disappears from device list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[3] Start IDE. Finds the Redlink probe? Or does this not happen until a debug session is started?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[4] Connect target USB cable to power target. [Presumably it appears in device list as DFU device but we don't care]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[5] Start a debug session in IDE -- which loads latest code on to target and applies 'remembered break points'. [Presumably, DFU device (target board) disappears from device list.]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[6] Start Host (PC side) USB Application&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[7] Shout Yippee! (or equivalent) and start debugging and testing etc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And if not, please explain in detail why and what the alternative should be.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: IDE = LPCXPresso 7&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, MIke&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551886#M12055</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Use 2xLPCLink-2 to Develop/Debug USB Device Firmware on an LPCLink-2 board.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551887#M12056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sun Mar 08 02:54:52 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Does this help?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Ffaq%2Flpcxpresso%2Fusing-lpclink2-as-lpc4370-eval" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/faq/lpcxpresso/using-lpclink2-as-lpc4370-eval&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551887#M12056</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:28:02Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Use 2xLPCLink-2 to Develop/Debug USB Device Firmware on an LPCLink-2 board.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551888#M12057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Sun Mar 08 02:57:36 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Absolutely not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you think I would not have researched and read everything before I have to ask questions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But thanks for replying at all.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551888#M12057</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:28:02Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Use 2xLPCLink-2 to Develop/Debug USB Device Firmware on an LPCLink-2 board.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551889#M12058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Sun Mar 08 04:43:50 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;Do you think I would not have researched and read everything before I have to ask questions.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You didn't say what you had research and I can't read your brain from here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The issue with LPC-Link2 (LPC43xx, strictly) is only that the dfu utility can't boot if two dfu-bootable devices with the same vid/pid are connected at the same time. The exact rules for whether a device will attempt to boot is described in the manual, but basically you can stop it by configuring boot pins. Do that, and there is no issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why not go and try it?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Use-2xLPCLink-2-to-Develop-Debug-USB-Device-Firmware/m-p/551889#M12058</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:28:03Z</dc:date>
    </item>
  </channel>
</rss>