<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: LPC1343 QuickStart USB connectivity problem</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551762#M12015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersrosvall on Thu Mar 22 04:06:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is an update on the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem has been traced back to a specific production batch of our LPC1343 QuickStart boards. There are exposed pads under the mini-B USB connector. On a few boards the metal shield of the mini-B USB connector can get contact with these pads. Typically when a (slightly big) connector is inserted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;All boards in distributor stock has been pulled back and fixed (only a very few number of boards were actually affected by this). Boards ordered after January 2012 are not affected. If you have a board with problems, please contact Embedded Artists support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kind Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anders Rosvall&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Embedded Artists AB&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:30:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:30:43Z</dc:date>
    <item>
      <title>LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551756#M12009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bitli on Sun Oct 16 12:33:09 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I cannot get an LPC 1343 QuickStart board (from Embedded Artists) to connect as an HID device to Windows.&amp;nbsp; I have reduced the program to a simple test that work well with the LCPXpresso board (equipped with a SoftConnect addition) but results in an Unrecognized Device on the quick start board (programmed via a 'cut' LCPXpresso LPC Link. The QuickStart is powered by the USB (as it does not receive the power from the LPC Link).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tried the following variations:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]Replaced the USB cable&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]Windows XP and Vista (same result)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]Added a wait of 2 seconds before asserting USB SoftConnect after reset. (The green led for soft connect is turned on when expected).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]Tried a second board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[*]Tried with another VendorId/ProductId than the 'Nxp demo' one.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/LIST]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The program behave as expected when run on the LpxExpresso 1343 board (it connects and is recongized as an HID device and data can be exchanged). &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I ran out of idea of things to try. Any clue ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-- bitli&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551756#M12009</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551757#M12010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Tsuneo on Sun Oct 16 14:08:29 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi bitli,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Run one of USB examples, first, which come with the QuickStart board. It confirms hardware integrity of the board around the USB circuit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Unfortunately, EA doesn't open the schematic of this board on their web. So, I can't point out the cause exactly. But I suppose your trouble would be caused by the difference of the extra port pin for D+ pull-up enable (SoftConnect).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Crystal frequency is the same, 12MHz, on both boards. It's fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tsuneo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551757#M12010</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551758#M12011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bitli on Mon Oct 17 09:14:04 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the schematic.&amp;nbsp; The Soft connect is very simple and uses a transistor to drive the resistor on the DP line. I reproduced the same function on the LPCXpresso and it works fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The board it is powered by the USB line (which is connected to the VBUS, something I also reproduced on the LPCXpresso). It has a reset circuit and a separate button to assert the PIO0_1 (boot enable), this is the only difference I see (except the connection to the EEProm). &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The program startd normally (it toggles some outputs and can see the signal).&amp;nbsp; The error message come only when the PIO0_s (soft connect) is asserted, as seen with the green led.&amp;nbsp; However maybe the boot code is doing something wrong.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My programs were started from the LCPEXpresso samples (there is no ROM driver HID example with the programs of the QuickStart).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551758#M12011</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551759#M12012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bitli on Tue Oct 18 10:28:40 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I continued investigations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The original QucikStart HID example program was downloaded to the quick start board, and resulted in the same error (USB device not recognized). Also in case of 'Reset+Boot' I have the same error.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Additionaly I tried with the USB HID example program on a 'fresh' PC to see if maybe it the USB driver was misconfigured on the previous ones. But the same error occurs (tried with two boards and two cables).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-- bitli&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551759#M12012</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551760#M12013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Tsuneo on Tue Oct 18 21:07:54 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;[I]&amp;gt; The original QucikStart HID example program was downloaded to the quick start board, and resulted in the same error (USB device not recognized).[/I]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As an EA's example doesn't run on the EA's board, contact to EA support on this issue. It may be a FAQ for them :-)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You may need some another spells, like erase entire FLASH to kill CRP. Does the QucikStart manual refer to anything?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tsuneo&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551760#M12013</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551761#M12014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bitli on Tue Oct 25 12:28:33 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In fact I have explored many other ways and got a lot of very helpful support from EA, including a board exchange.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Unfortunately so far without success (replacing board, OS, computer,&amp;nbsp; cable, ... does not seem to have an impact, USB just don't work here).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Still exploring&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-- bitli&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551761#M12014</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1343 QuickStart USB connectivity problem</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551762#M12015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andersrosvall on Thu Mar 22 04:06:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is an update on the issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem has been traced back to a specific production batch of our LPC1343 QuickStart boards. There are exposed pads under the mini-B USB connector. On a few boards the metal shield of the mini-B USB connector can get contact with these pads. Typically when a (slightly big) connector is inserted.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;All boards in distributor stock has been pulled back and fixed (only a very few number of boards were actually affected by this). Boards ordered after January 2012 are not affected. If you have a board with problems, please contact Embedded Artists support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Kind Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anders Rosvall&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Embedded Artists AB&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1343-QuickStart-USB-connectivity-problem/m-p/551762#M12015</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:30:43Z</dc:date>
    </item>
  </channel>
</rss>