<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lpcxpresso: debugging external target does not work. in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551277#M11784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by s.achterop@rug.nl on Wed Aug 29 13:23:30 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the response.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had JTAG_RESET connected to TRST (pin 4) and not to RESET_N as you said and I now also see in the schematics of the LPC1768-lpcxpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; Thanks for the help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sietse&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:08:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:08:39Z</dc:date>
    <item>
      <title>lpcxpresso: debugging external target does not work.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551275#M11782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by s.achterop@rug.nl on Tue Aug 28 10:34:15 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear list,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I cannot debug my custom lpc1768 board with the LPC-Link part of a LPCXpresso (LPC1114)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I separated the LPC1114 from the LPCXPRESSO and connected the lpc-link to my target.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I did not use the 10-pins header, but used the connections from the interface to the LPC1114 side&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;of my lpcxpresso. So signal RTCK is not used, but that is OK. And all 5 JTAG connections are properly&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;connected to the lpc1768 (pin 1 to 5) on my custom board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on Linux and the following happens:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;$ crt_emu_cm3_nxp -info-scan&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Ni: LPCXpresso Debug Driver v4.0 (Dec 12 2011 10:43:04)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Ee(05). No matching emulator found - make sure power is on and not in use already.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;$ crt_emu_cm3_nxp -info-emu&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ni: LPCXpresso Debug Driver v4.0 (Dec 12 2011 10:43:04)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0 Emulators available:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It seems as if the lpc1768 is not recognized, but each time I boot the lpc1768 in bootmode using&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;pin P2_10 is seems that it can be flashed ONE SINGLE time!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So the lpc1768 seems to be working at least partly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Here the first two invocations of the bootloader AFTER starting the ISP command handler using P2_10:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;$&amp;nbsp; crt_emu_cm3_nxp&amp;nbsp; -2 -pLPC1768 -vendor=NXP -wire=winusb -flash-load-exec=ledjes.bin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Ni: LPCXpresso Debug Driver v4.0 (Dec 12 2011 10:43:04)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Looked for chip XML file in /usr/local/lpcxpresso_4.1.5_187/lpcxpresso/bin/LPC1768.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Looked for vendor directory XML file in /usr/local/lpcxpresso_4.1.5_187/lpcxpresso/bin/nxp_directory.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Found generic directory XML file in /usr/local/lpcxpresso_4.1.5_187/lpcxpresso/bin/crt_directory.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Emu(0): Conn&amp;amp;Reset. DpID: 2BA01477. Info: LPCLINK_1_1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Packet delay: 0&amp;nbsp; Poll delay: 0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: NXP: LPC1768&amp;nbsp; Part ID: 0x26013F37&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nt: Connected: was_reset=true. was_stopped=false&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Cr:v Registered license, download limit of 128K&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nt: Loading binary file 'ledjes.bin' at location 00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nt: Writing 660 bytes to 0000 in Flash (assumed clock: 14.748MHz)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nt: Verified-same page 0-0 with 660 bytes in 260msec&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nt: Flash write Done&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: nSRST assert (if available)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Executing in bootloader.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nt:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: nSRST assert (if available)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Executing in bootloader.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;$&amp;nbsp; crt_emu_cm3_nxp&amp;nbsp; -2 -pLPC1768 -vendor=NXP -wire=winusb -flash-load-exec=ledjes.bin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Ni: LPCXpresso Debug Driver v4.0 (Dec 12 2011 10:43:0&amp;nbsp;&amp;nbsp; Nc: Looked for chip XML file in /usr/local/lpcxpresso_4.1.5_187/lpcxpresso/bin/LPC1768.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Looked for vendor directory XML file in /usr/local/lpcxpresso_4.1.5_187/lpcxpresso/bin/nxp_directory.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Nc: Found generic directory XML file in /usr/local/lpcxpresso_4.1.5_187/lpcxpresso/bin/crt_directory.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Xw:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Ed:02: Failed on connect: Ep(04). Cannot halt processor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Et: Emu(0): Conn&amp;amp;Reset. Was: None. DpID: 2BA01477. Info: LPCLINK_1_1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Error 0: (null)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Last sticky: 16. AIndex: 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; MemAp selected: 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Speed test resends: 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Packet delay: 0&amp;nbsp; Poll delay: 0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The first time seems OK, but after that the target cannot be used anymore.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Using gdb gives something similar, the first time it seems to flash ok, but after the first "stepi" it does&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;not return.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is not related to file to be flashed, because that works properly on a lpcxpresso with a lpc1768.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It could be that my hardware is broken, but I don't think so.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone has an idea what is wrong, or how to test any further?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; Thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sietse Achterop&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551275#M11782</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: lpcxpresso: debugging external target does not work.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551276#M11783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Tue Aug 28 11:11:58 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;&lt;SPAN&gt;Quote: &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:s.achterop@rug.nl"&gt;s.achterop@rug.nl&lt;/A&gt;&lt;/STRONG&gt;&lt;BR /&gt;And all 5 JTAG connections are properly connected to the lpc1768 (pin 1 to 5) on my custom board.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sorry, can't follow you :confused: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#1 Connect SWD as described in #9 of: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?p=8311&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Especially J4-11 connected to LPC1768-Pin17 (Reset_N) will help you get your SWD working&amp;nbsp; :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#2 Enable vector catch as described here: &lt;/SPAN&gt;&lt;A href="http://"&gt;http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:08:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551276#M11783</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:08:38Z</dc:date>
    </item>
    <item>
      <title>Re: lpcxpresso: debugging external target does not work.</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551277#M11784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by s.achterop@rug.nl on Wed Aug 29 13:23:30 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the response.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I had JTAG_RESET connected to TRST (pin 4) and not to RESET_N as you said and I now also see in the schematics of the LPC1768-lpcxpresso.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; Thanks for the help!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Sietse&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:08:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/lpcxpresso-debugging-external-target-does-not-work/m-p/551277#M11784</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:08:39Z</dc:date>
    </item>
  </channel>
</rss>