<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC4330 SPIFI Data save from M0/M4 application in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550474#M11442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by demarchidaniele on Wed Aug 29 05:49:02 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am porting a project from PIC32 to LPC4330 :D.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The port is near to be terminated but I am in trouble with data saving into flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For tests I am using LPC4330 Xplorer that has a SPIFI flash S25FL032P.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The idea is to reserve a portion of flash memory for data storage.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have modified the memory configuration with a PROGAREA_REGION intended to be used for read and write from the M0 or M4 application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Address and size is not yet defined, for the moment a size of 0x10000 byte is enough (see picture).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've looked for an example but everything seems not working or incomplete.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can somebody suggest a working example for it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Second question: while programming the external flash is possible to continue execution from another region of the same external Flash?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPCXpresso Version: v4.2.4 [Build 267] [2012-07-11]&amp;nbsp; for MAC OS X&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:08:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:08:57Z</dc:date>
    <item>
      <title>LPC4330 SPIFI Data save from M0/M4 application</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550474#M11442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by demarchidaniele on Wed Aug 29 05:49:02 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am porting a project from PIC32 to LPC4330 :D.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The port is near to be terminated but I am in trouble with data saving into flash.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For tests I am using LPC4330 Xplorer that has a SPIFI flash S25FL032P.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The idea is to reserve a portion of flash memory for data storage.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have modified the memory configuration with a PROGAREA_REGION intended to be used for read and write from the M0 or M4 application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Address and size is not yet defined, for the moment a size of 0x10000 byte is enough (see picture).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've looked for an example but everything seems not working or incomplete.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can somebody suggest a working example for it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Second question: while programming the external flash is possible to continue execution from another region of the same external Flash?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPCXpresso Version: v4.2.4 [Build 267] [2012-07-11]&amp;nbsp; for MAC OS X&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550474#M11442</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4330 SPIFI Data save from M0/M4 application</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550475#M11443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by NXP_Europe on Thu Aug 30 13:52:40 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello demarchidaniele,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Did you check the &lt;/SPAN&gt;&lt;A href="http://http://www.lpcware.com"&gt;www.lpcware.com&lt;/A&gt;&lt;SPAN&gt; website?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;see:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.lpcware.com/gfiles/devper/lpc43xx&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;see:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.lpcware.com/content/nxpfile/an11177-inter-processor-communication-lpc43xx&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;see:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://www.lpcware.com/content/nxpfile/an11206-using-spifi-lpc1800-and-lpc4300&lt;/A&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope this solves your problem.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550475#M11443</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:08:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4330 SPIFI Data save from M0/M4 application</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550476#M11444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by demarchidaniele on Thu Aug 30 14:47:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for&amp;nbsp; your support.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I see this docs, i will try.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;de marchi daniele&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC4330-SPIFI-Data-save-from-M0-M4-application/m-p/550476#M11444</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:08:58Z</dc:date>
    </item>
  </channel>
</rss>