<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPCXpresso and GCC?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-GCC/m-p/550132#M11289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Mark_O on Fri Feb 12 19:40:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've looked in both the KnowledgeBase and done a search of the Forum, but was unable to find the answer to a question I had.&amp;nbsp; Regarding this, from the main page on LPCXpresso:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"[I]LPCXpresso is based on Eclipse with many LPC-specific enhancements. It also features the latest version of the industry standard GNU tool chain with a proprietary optimized C library...[/I]"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is C the only language from the GNU Compiler Collection that is supported?&amp;nbsp; Or are the rest as well?&amp;nbsp; I.e., C++, Objective-C, and plug-in front-ends like Pascal?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Mark&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:40:04 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:40:04Z</dc:date>
    <item>
      <title>LPCXpresso and GCC?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-GCC/m-p/550132#M11289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Mark_O on Fri Feb 12 19:40:46 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I've looked in both the KnowledgeBase and done a search of the Forum, but was unable to find the answer to a question I had.&amp;nbsp; Regarding this, from the main page on LPCXpresso:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"[I]LPCXpresso is based on Eclipse with many LPC-specific enhancements. It also features the latest version of the industry standard GNU tool chain with a proprietary optimized C library...[/I]"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is C the only language from the GNU Compiler Collection that is supported?&amp;nbsp; Or are the rest as well?&amp;nbsp; I.e., C++, Objective-C, and plug-in front-ends like Pascal?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Mark&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-GCC/m-p/550132#M11289</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso and GCC?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-GCC/m-p/550133#M11290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Sat Feb 13 03:11:41 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Only C is supported directly in the IDE, although the C++ compiler is also provided. No other languages are supported.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-and-GCC/m-p/550133#M11290</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:40:05Z</dc:date>
    </item>
  </channel>
</rss>