<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックMaximum Allowable Torquage?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/549998#M11224</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by woodchuck on Mon Aug 02 13:08:17 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What clock rates do the 1114, 1343, and 1768 operate at, by default, in the LPCxpresso environment? Which initialization file specifies this value?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:05:54 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:05:54Z</dc:date>
    <item>
      <title>Maximum Allowable Torquage?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/549998#M11224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by woodchuck on Mon Aug 02 13:08:17 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;What clock rates do the 1114, 1343, and 1768 operate at, by default, in the LPCxpresso environment? Which initialization file specifies this value?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/549998#M11224</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum Allowable Torquage?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/549999#M11225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Aug 03 01:33:39 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;From memory, 48MHz (LPC11), 72MHz (LPC13) and 100MHz (LPC17) are the default settings used. These are set up in the [FONT=Courier New][SIZE=2]system_LPC[I]nn[/I]xx.c[/SIZE][/FONT] file (replace [FONT=Courier New][SIZE=2][I]nn[/I][/SIZE][/FONT] with part number) within the appropriate CMSIS library project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you access the[FONT=Courier New][SIZE=2] SystemCoreClock[/SIZE][/FONT] variable within your code base, then you can see what clock speed has been set up. [Note that if you don't actually reference SystemCoreClock from your code, the linker will normally remove it from the final image - so you won't then be able to see it within the debugger.]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you want to change clock speeds, then I would advise using the PLL spreadsheet NXP have available:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC17...&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://ics.nxp.com/support/documents/microcontrollers/xls/lpc17xx.pll.calculator.xls&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC11...&lt;/SPAN&gt;&lt;BR /&gt;&lt;A href="http://"&gt;http://knowledgebase.nxp.com/showthread.php?t=337&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/549999#M11225</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:55Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum Allowable Torquage?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/550000#M11226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by woodchuck on Tue Aug 03 13:14:00 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Perfect!&amp;nbsp; Many thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Maximum-Allowable-Torquage/m-p/550000#M11226</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:56Z</dc:date>
    </item>
  </channel>
</rss>