<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 LPCxpresso LPC1769 and TCP/IP</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549467#M10985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by markustmaier on Tue Sep 11 09:25:16 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm looking for an easy implementation of a TCP/IP stack for the LPCxpresso LPC1769 and Baseboard from Embedded Artists. I aim to use simple TCP send and receive commands to communicate with a motor controller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have to communicate with three of these motor controllers, so I should be able to open three different connections. The commands are realy simple like "HORM". &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Which stack is the best for this application? Speed is not a issue. Which stack can be understand easier? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- lwIP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- uIP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- EasyWeb&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there anybody who has source code for one of these stacks? I'm new to ethernet and I like to have two little functions: TCP_Send and TCP_Receive where I can send and receive strings via TCP. There is enough to do with the coding of the other parts, so the ethernet part should be as easy as possible.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Markus&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:05:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:05:50Z</dc:date>
    <item>
      <title>LPCxpresso LPC1769 and TCP/IP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549467#M10985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by markustmaier on Tue Sep 11 09:25:16 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm looking for an easy implementation of a TCP/IP stack for the LPCxpresso LPC1769 and Baseboard from Embedded Artists. I aim to use simple TCP send and receive commands to communicate with a motor controller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have to communicate with three of these motor controllers, so I should be able to open three different connections. The commands are realy simple like "HORM". &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Which stack is the best for this application? Speed is not a issue. Which stack can be understand easier? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- lwIP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- uIP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- EasyWeb&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there anybody who has source code for one of these stacks? I'm new to ethernet and I like to have two little functions: TCP_Send and TCP_Receive where I can send and receive strings via TCP. There is enough to do with the coding of the other parts, so the ethernet part should be as easy as possible.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Markus&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549467#M10985</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso LPC1769 and TCP/IP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549468#M10986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by daniel.widyanto on Fri Sep 28 01:04:26 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Markus,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See this app note: &lt;/SPAN&gt;&lt;A href="http://http://www.nxp.com/documents/other/uip_webserver_src_lpc1700.zip"&gt;http://www.nxp.com/documents/other/uip_webserver_src_lpc1700.zip&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549468#M10986</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso LPC1769 and TCP/IP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549469#M10987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by markustmaier on Fri Nov 02 03:29:57 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks for the link. I've already looked at the app note. But I don't understand how I can send and receive TCP strings.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a easy way to do this? Maybe an idea where I can look at those funtions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549469#M10987</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso LPC1769 and TCP/IP</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549470#M10988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Fri Nov 02 03:52:05 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: markustmaier&lt;/STRONG&gt;&lt;BR /&gt;Is there a easy way to do this? &lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;AFAIK No :o&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;EasyWeb is including http and therefore TCP. To send / receive data it's useful to understand what TCP is and how it works. So it can be useful to read TCP parts of EasyWeb. If you are looking for a simple way, try mbed :)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCxpresso-LPC1769-and-TCP-IP/m-p/549470#M10988</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:05:52Z</dc:date>
    </item>
  </channel>
</rss>