<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCXpresso Board With CAN Controller? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549202#M10870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rtos on Sun Feb 14 06:53:44 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I think I found the answer in another post:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;The mbed board does not have debugger connections on it, so it cannot be&amp;nbsp; connected to an external debugger such as the LPCXpresso LPC-LINK.&amp;nbsp; However the LPCXpresso IDE can generate binary files which can be&amp;nbsp; programmed into the mbed board over the USB connection. &lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:37:41 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:37:41Z</dc:date>
    <item>
      <title>LPCXpresso Board With CAN Controller?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549199#M10867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rtos on Sat Feb 13 16:38:31 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there an LPCXpresso board that has a [B]CAN Controller[/B]? Something with the LPC1764 or similar?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If not, is there a drop-in compatible LPC with a CAN Controller that I could swap onto the LPCXpresso LPC 1343 board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549199#M10867</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso Board With CAN Controller?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549200#M10868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by annodomini2 on Sun Feb 14 03:35:27 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Not at this time, NXP are doing some LPC11 series with CAN later this year.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There's the MBED if you want CAN.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or a number of other LPC17xx series dev boards with CAN.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Unless an ARM7 is acceptable then there's devices such as the LPC2109. LPC2129&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Other manufacturers include STM32F103&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or conversely you can add an SPI CAN controller to the LPC11 or LPC13&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549200#M10868</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso Board With CAN Controller?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549201#M10869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rtos on Sun Feb 14 06:25:49 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: annodomini2&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;There's the MBED if you want CAN.&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&amp;nbsp; Can the MBED be used with the LPCXpresso programmer and compiler?&amp;nbsp; Or is it locked into using their online compiler?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549201#M10869</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso Board With CAN Controller?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549202#M10870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rtos on Sun Feb 14 06:53:44 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I think I found the answer in another post:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN&gt;The mbed board does not have debugger connections on it, so it cannot be&amp;nbsp; connected to an external debugger such as the LPCXpresso LPC-LINK.&amp;nbsp; However the LPCXpresso IDE can generate binary files which can be&amp;nbsp; programmed into the mbed board over the USB connection. &lt;/SPAN&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:37:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549202#M10870</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:37:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso Board With CAN Controller?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549203#M10871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by annodomini2 on Mon Feb 15 16:08:27 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yup, mbed has a cloud based online IDE and compiler with a reasonable library set.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or you can use Eclipse and YAGARTO or one of the other ARM compiler toolchains.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes the JTAG cannot be used with an mbed the JTAG interface is used by its programming interface.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCXpresso-Board-With-CAN-Controller/m-p/549203#M10871</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:37:42Z</dc:date>
    </item>
  </channel>
</rss>